DAC_InitChannel_TypeDef Struct ReferenceEMLIB > DAC

DAC channel init structure.

Definition at line 186 of file em_dac.h .

#include < em_dac.h >

Data Fields

bool enable
bool prsEnable
DAC_PRSSEL_TypeDef prsSel
bool refreshEnable

Field Documentation

bool DAC_InitChannel_TypeDef::enable

Enable channel.

Definition at line 188 of file em_dac.h .

Referenced by DAC_InitChannel() .

bool DAC_InitChannel_TypeDef::prsEnable

Peripheral reflex system trigger enable. If false, channel is triggered by writing to CHnDATA.

Definition at line 194 of file em_dac.h .

Referenced by DAC_InitChannel() .

DAC_PRSSEL_TypeDef DAC_InitChannel_TypeDef::prsSel

Peripheral reflex system trigger selection. Only applicable if prsEnable is enabled.

Definition at line 206 of file em_dac.h .

Referenced by DAC_InitChannel() .

bool DAC_InitChannel_TypeDef::refreshEnable

Enable/disable automatic refresh of channel. Refresh interval must be defined in common control init, please see DAC_Init() .

Definition at line 200 of file em_dac.h .

Referenced by DAC_InitChannel() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_dac.h