LCD_TypeDef Struct ReferenceDevices > EFM32G_LCD
Definition at line 48
of file efm32g_lcd.h
.
Data Fields | |
__IOM uint32_t | AREGA |
__IOM uint32_t | AREGB |
__IOM uint32_t | BACTRL |
__IOM uint32_t | CTRL |
__IOM uint32_t | DISPCTRL |
__IOM uint32_t | FREEZE |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
uint32_t | RESERVED0 [5] |
__IOM uint32_t | SEGD0H |
__IOM uint32_t | SEGD0L |
__IOM uint32_t | SEGD1H |
__IOM uint32_t | SEGD1L |
__IOM uint32_t | SEGD2H |
__IOM uint32_t | SEGD2L |
__IOM uint32_t | SEGD3H |
__IOM uint32_t | SEGD3L |
__IOM uint32_t | SEGEN |
__IM uint32_t | STATUS |
__IM uint32_t | SYNCBUSY |
Field Documentation
__IOM uint32_t LCD_TypeDef::AREGA |
Animation Register A
Definition at line 54
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::AREGB |
Animation Register B
Definition at line 55
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::BACTRL |
Blink and Animation Control Register
Definition at line 52
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::DISPCTRL |
Display Control Register
Definition at line 50
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::FREEZE |
Freeze Register
Definition at line 70
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::IEN |
Interrupt Enable Register
Definition at line 59
of file efm32g_lcd.h
.
__IM uint32_t LCD_TypeDef::IF |
Interrupt Flag Register
Definition at line 56
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 58
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 57
of file efm32g_lcd.h
.
uint32_t LCD_TypeDef::RESERVED0[5] |
Reserved for future use
Definition at line 60
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD0H |
Segment Data High Register 0
Definition at line 65
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD0L |
Segment Data Low Register 0
Definition at line 61
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD1H |
Segment Data High Register 1
Definition at line 66
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD1L |
Segment Data Low Register 1
Definition at line 62
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD2H |
Segment Data High Register 2
Definition at line 67
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD2L |
Segment Data Low Register 2
Definition at line 63
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD3H |
Segment Data High Register 3
Definition at line 68
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD3L |
Segment Data Low Register 3
Definition at line 64
of file efm32g_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGEN |
Segment Enable Register
Definition at line 51
of file efm32g_lcd.h
.
__IM uint32_t LCD_TypeDef::STATUS |
Status Register
Definition at line 53
of file efm32g_lcd.h
.
__IM uint32_t LCD_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 71
of file efm32g_lcd.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32G/Include/
efm32g_lcd.h