MSDSCSI_RequestSense_TypeDef Struct ReferenceKit Drivers > Msd
SCSI Request Sense Command Descriptor Block (CDB) typedef.
Definition at line 126
of file msdscsi.h
.
#include <
msdscsi.h
>
Data Fields | |
struct { | |
uint8_t Desc: 1 | |
uint8_t Reserved1: 7 | |
}; | |
uint8_t | AllocationLength |
uint8_t | Control |
uint8_t | OpCode |
uint8_t | Reserved2 |
uint8_t | Reserved3 |
Field Documentation
uint8_t MSDSCSI_RequestSense_TypeDef::AllocationLength |
Number of sense data bytes requested.
Definition at line 134
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSense_TypeDef::Control |
Control byte.
Definition at line 135
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSense_TypeDef::Desc |
Descriptor format.
Definition at line 129
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSense_TypeDef::OpCode |
Command opcode.
Definition at line 127
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSense_TypeDef::Reserved1 |
Reserved, expect 0.
Definition at line 130
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSense_TypeDef::Reserved2 |
Reserved, expect 0.
Definition at line 132
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSense_TypeDef::Reserved3 |
Reserved, expect 0.
Definition at line 133
of file msdscsi.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/hardware/kit/common/drivers/
msdscsi.h