msdd.h File Reference
Mass Storage class Device (MSD) driver.
- Version
- 5.4.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file msdd.h
.
Data Structures | |
struct | MSDD_CmdStatus_TypeDef |
Status info for one BOT CBW -> Data I/O -> CSW cycle. | |
Macros | |
#define | MEDIA_BUFSIZ 4096 |
Functions | |
bool | MSDD_Handler (void) |
Serve the MSD state machine. This function should be called on a regular basis from your main loop. It cannot be called from within an interrupt handler. | |
void | MSDD_Init (int activityLedPort, uint32_t activityLedPin) |
Initialize MSD device. | |
int | MSDD_SetupCmd (const USB_Setup_TypeDef *setup) |
Called whenever a USB setup command is received. This function overrides standard CLEAR_FEATURE commands, and implements MSD class commands "Bulk-Only Mass Storage Reset" and "Get Max LUN". | |
void | MSDD_StateChangeEvent (USBD_State_TypeDef oldState, USBD_State_TypeDef newState) |
Called whenever the USB device has changed its device state. | |