touch.c File Reference
EFM32GG_DK3750, Touch panel driver.
- Version
- 5.4.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file touch.c
.
#include <stdlib.h>
#include <string.h>
#include "em_device.h
"
#include "em_adc.h
"
#include "em_gpio.h
"
#include "em_cmu.h
"
#include "touch.h
"
#include "calibrate.h"
#include "bsp.h
"
#include "i2cspm.h
"
#include "eeprom.h
"
Macros | |
#define | ADC_X adcSingleInpCh1 |
#define | ADC_Y adcSingleInpCh4 |
#define | TOUCH_X1_PIN 5 |
#define | TOUCH_X1_PORT gpioPortD |
#define | TOUCH_X2_PIN 4 |
#define | TOUCH_X2_PORT gpioPortD |
#define | TOUCH_Y1_PIN 3 |
#define | TOUCH_Y1_PORT gpioPortD |
#define | TOUCH_Y2_PIN 1 |
#define | TOUCH_Y2_PORT gpioPortD |
Enumerations | |
enum | TOUCH_State_TypeDef { TOUCH_INIT, TOUCH_CHECK_PRESS, TOUCH_MEASURE_X, TOUCH_MEASURE_Y } |
Functions | |
void | ADC0_IRQHandler (void) |
Interrupt handler is executed with frequency ~28Hz when panel is not pressed and with frequency ~140Hz when panel is pressed - this will give ~50 readings per second. | |
int | TOUCH_CalibrationTable (POINT *displayPtr, POINT *screenPtr) |
Set calibration table. | |
void | TOUCH_CallUpcall (void) |
Function that calls registered upcall. | |
TOUCH_Pos_TypeDef * | TOUCH_GetPos (void) |
Returns current touch position and state. | |
void | TOUCH_Init (TOUCH_Config_TypeDef *config) |
Initialize touch panel driver. | |
int | TOUCH_IsBusy (void) |
Check status of the touch panel. | |
void | TOUCH_RecalculatePosition (volatile TOUCH_Pos_TypeDef *pos) |
Convert ADC readings into XY position. | |
void | TOUCH_RegisterUpcall (TOUCH_Upcall_TypeDef *new_upcall) |
Register upcall which will be call every position or state change. | |
int | TOUCH_StateChanged (void) |
Check if cursor state changed (down or move) | |
Variables | |
MATRIX | calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 } |
Macro Definition Documentation
#define ADC_X adcSingleInpCh1 |
#define ADC_Y adcSingleInpCh4 |
Input channel 4
Definition at line 37
of file touch.c
.
Referenced by ADC0_IRQHandler(), and TOUCH_Init().
#define TOUCH_X1_PIN 5 |
#define TOUCH_X1_PORT gpioPortD |
#define TOUCH_X2_PIN 4 |
#define TOUCH_X2_PORT gpioPortD |
#define TOUCH_Y1_PIN 3 |
#define TOUCH_Y1_PORT gpioPortD |
#define TOUCH_Y2_PIN 1 |
#define TOUCH_Y2_PORT gpioPortD |
Enumeration Type Documentation
enum TOUCH_State_TypeDef |
touch driver states
Definition at line 50
of file touch.c
.
Function Documentation
void TOUCH_RecalculatePosition | ( | volatile TOUCH_Pos_TypeDef * | pos | ) |
Convert ADC readings into XY position.
- Parameters
-
[in] pos
Pointer to position structure
Definition at line 158
of file touch.c
.
References TOUCH_Pos_TypeDef::adcx, TOUCH_Pos_TypeDef::adcy, calibrationMatrix, TOUCH_Pos_TypeDef::pen, TOUCH_Pos_TypeDef::x, and TOUCH_Pos_TypeDef::y.
Referenced by ADC0_IRQHandler().
int TOUCH_StateChanged | ( | void |
| ) |
Check if cursor state changed (down or move)
- Returns
- 1 if the cursor state has changed
Definition at line 201
of file touch.c
.
References TOUCH_Pos_TypeDef::pen, TOUCH_Pos_TypeDef::x, and TOUCH_Pos_TypeDef::y.
Referenced by ADC0_IRQHandler().
Variable Documentation
MATRIX calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 } |
Calibration table
Definition at line 70
of file touch.c
.
Referenced by TOUCH_CalibrationTable(), and TOUCH_RecalculatePosition().