TftKit Drivers

Functions

void SPI_TFT_Init (void)
SPI_TFT_Init Initialize SPI interface to TFT-LCD SSD2119 controller.
void SPI_TFT_WriteRegister (uint8_t reg, uint16_t data)
SPI_TFT_Write Write registers/data to SSD2119 controller.
bool TFT_AddressMappedInit (void)
TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
void TFT_DirectGPIOConfig (void)
GPIO configuration for TFT direct drive.
bool TFT_DirectInit (const EBI_TFTInit_TypeDef *tftInit)
TFT initialize or reinitialize Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)

Function Documentation

void SPI_TFT_Init ( void )

SPI_TFT_Init Initialize SPI interface to TFT-LCD SSD2119 controller.

Note
To enable access, be sure to call the functions BSP_PeripheralAccess(BSP_TFT, enable); before using this interface.

Definition at line 45 of file tftspi.c .

References CMU_ClockEnable() , cmuClock_GPIO , cmuClock_HFPER , cmuClock_USART1 , GPIO_PinModeSet() , gpioModeInput , gpioModePushPull , USART1 , USART_InitSync() , USART_Reset() , USART_ROUTE_CLKPEN , USART_ROUTE_LOCATION_LOC1 , USART_ROUTE_RXPEN , and USART_ROUTE_TXPEN .

void SPI_TFT_WriteRegister ( uint8_t reg,
uint16_t data
)

SPI_TFT_Write Write registers/data to SSD2119 controller.

Parameters
reg Register to write to
data 16-bit data to write into register
Note
It's not possible to read back register value through SSD2119 SPI interface, so no SPI_TFT_ReadRegister function is implemented

Definition at line 80 of file tftspi.c .

References GPIO_PinOutClear() , GPIO_PinOutSet() , USART1 , USART_CTRL_BIT8DV , USART_Rx() , and USART_Tx() .

bool TFT_AddressMappedInit ( void )

TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)

Returns
true if we should redraw into buffer, false if BC has control over display

Definition at line 36 of file tftamapped.c .

References BC_ARB_CTRL_EBI , BC_REGISTER , BC_SPI_DEMUX_SLAVE_AUDIO , BC_SPI_DEMUX_SLAVE_DISPLAY , BC_SSD2119_BASE , BC_UIF_AEM_EFM , BSP_Display_EBI , BSP_Display_Mode8080 , BSP_Display_PowerDisable , BSP_Display_PowerEnable , BSP_Display_ResetAssert , BSP_Display_ResetRelease , BSP_DisplayControl() , BSP_RegisterRead() , BSP_RegisterWrite() , runOnce , and SystemCoreClockGet() .

bool TFT_DirectInit ( const EBI_TFTInit_TypeDef * tftInit )

TFT initialize or reinitialize Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)

Parameters
[in] tftInit Pointer to EBI TFT initialization structure
Returns
true if we should redraw into buffer, false if BC has control over display

Definition at line 52 of file tftdirect.c .

References BC_ARB_CTRL_EBI , BC_REGISTER , BC_UIF_AEM_EFM , BSP_Display_EBI , BSP_Display_ModeGeneric , BSP_Display_PowerDisable , BSP_Display_PowerEnable , BSP_Display_ResetAssert , BSP_Display_ResetRelease , BSP_DisplayControl() , BSP_PeripheralAccess() , BSP_RegisterRead() , BSP_TFT , EBI_BANK2 , EBI_BankAddress() , EBI_TFTInit() , runOnce , SystemCoreClockGet() , and TFT_DirectGPIOConfig() .