DMA_DESCRIPTOR_TypeDef Struct ReferenceDevices > EFM32GG_DMA_DESCRIPTOR

Definition at line 47 of file efm32gg_dma_descriptor.h .

Data Fields

__IOM uint32_t CTRL
__IOM void *__IOM DSTEND
__IOM void *__IOM SRCEND
__IOM uint32_t USER

Field Documentation

__IOM uint32_t DMA_DESCRIPTOR_TypeDef::CTRL

DMA control register

Definition at line 52 of file efm32gg_dma_descriptor.h .

Referenced by DMA_ActivateScatterGather() , DMA_CfgDescr() , DMA_CfgDescrScatterGather() , and DMA_RefreshPingPong() .

__IOM void* __IOM DMA_DESCRIPTOR_TypeDef::DSTEND

DMA destination address end

Definition at line 51 of file efm32gg_dma_descriptor.h .

Referenced by DMA_ActivateScatterGather() , DMA_CfgDescrScatterGather() , and DMA_RefreshPingPong() .

__IOM void* __IOM DMA_DESCRIPTOR_TypeDef::SRCEND

DMA source address end

Definition at line 50 of file efm32gg_dma_descriptor.h .

Referenced by DMA_ActivateScatterGather() , DMA_CfgDescrScatterGather() , and DMA_RefreshPingPong() .

__IOM uint32_t DMA_DESCRIPTOR_TypeDef::USER

DMA padding register, available for user

Definition at line 53 of file efm32gg_dma_descriptor.h .

Referenced by DMA_ActivateScatterGather() , DMA_CfgChannel() , and DMA_CfgDescrScatterGather() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG/Include/ efm32gg_dma_descriptor.h