DMA_CfgRect_TypeDef Struct ReferenceEMLIB > DMA
Configuration structure for rectangular copy.
Definition at line 247
of file em_dma.h
.
#include <
em_dma.h
>
Data Fields | |
uint16_t | dstStride |
uint16_t | height |
uint16_t | srcStride |
Field Documentation
uint16_t DMA_CfgRect_TypeDef::dstStride |
DMA channel destination stride (width of destination image, distance between lines).
Definition at line 249
of file em_dma.h
.
Referenced by DMA_CfgRect().
uint16_t DMA_CfgRect_TypeDef::height |
uint16_t DMA_CfgRect_TypeDef::srcStride |
DMA channel source stride (width of source image, distance between lines).
Definition at line 251
of file em_dma.h
.
Referenced by DMA_CfgRect().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_dma.h