retargetserial.c File Reference
Provide stdio retargeting to USART/UART or LEUART.
- Version
- 5.5.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file retargetserial.c
.
#include <stdio.h>
#include "em_device.h
"
#include "em_cmu.h
"
#include "em_core.h
"
#include "em_gpio.h
"
#include "retargetserial.h
"
#include "retargetserialconfig.h"
Macros | |
#define | _GENERIC_UART_STATUS_IDLE LEUART_STATUS_TXC |
#define | RXBUFSIZE 8 |
Functions | |
static void | disableRxInterrupt () |
Disable RX interrupt. | |
static void | enableRxInterrupt () |
Enable RX interrupt. | |
void | RETARGET_IRQ_NAME (void) |
UART/LEUART IRQ Handler. | |
int | RETARGET_ReadChar (void) |
Receive a byte from USART/LEUART and put into global buffer. | |
void | RETARGET_SerialCrLf (int on) |
UART/LEUART toggle LF to CRLF conversion. | |
bool | RETARGET_SerialEnableFlowControl (void) |
Enable hardware flow control. (RTS + CTS) | |
void | RETARGET_SerialFlush (void) |
Flush UART/LEUART. | |
void | RETARGET_SerialInit (void) |
Intializes UART/LEUART. | |
int | RETARGET_WriteChar (char c) |
Transmit single byte to USART/LEUART. | |
Variables | |
static bool | initialized = false |
static uint8_t | LFtoCRLF = 0 |
static volatile uint8_t | rxBuffer [RXBUFSIZE] |
static volatile int | rxCount = 0 |
static volatile int | rxReadIndex = 0 |
static volatile int | rxWriteIndex = 0 |