caplesense.c File Reference
Capacitive sense driver.
- Version
- 5.5.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
caplesense.c
.
#include "
em_device.h
"
#include "
caplesense.h
"
#include "
em_emu.h
"
#include "
em_acmp.h
"
#include "
em_assert.h
"
#include "
em_cmu.h
"
#include "
em_gpio.h
"
#include "
em_core.h
"
#include "
em_lesense.h
"
#include "caplesenseconfig.h"
Functions |
|
| uint32_t | CAPLESENSE_getNormalizedVal (uint8_t channel) |
|
Get the current normalized channelValue for a channel.
|
|
| uint8_t | CAPLESENSE_getSegmentChannel (uint8_t capSegment) |
|
Get the channelValue for a sensor segment.
|
|
| int32_t | CAPLESENSE_getSliderPosition (void) |
|
Get the position of the slider.
|
|
| uint32_t | CAPLESENSE_getVal (uint8_t channel) |
|
Get the current channelValue for a channel.
|
|
| void | CAPLESENSE_Init (bool sleep) |
|
Initializes the capacative sense system without LESENSE.
|
|
| void | CAPLESENSE_setupACMP (void) |
|
Setup the ACMP.
|
|
| void | CAPLESENSE_setupCallbacks (void(*scanCb)(void), void(*chCb)(void)) |
|
LESENSE callback setup.
|
|
| void | CAPLESENSE_setupCMU (void) |
|
Setup the CMU.
|
|
| void | CAPLESENSE_setupGPIO (void) |
|
Setup the GPIO.
|
|
| void | CAPLESENSE_setupLESENSE (bool sleep) |
|
Setup the LESENSE for capavitive sensing.
|
|
| void | CAPLESENSE_Sleep (void) |
|
Send the capacative sense system to sleep mode.
|
|
| void | LESENSE_IRQHandler (void) |
|
LESENSE interrupt handler.
|
|
Variables |
|
| static volatile uint32_t | channelMaxValues [LESENSE_CHANNELS] |
|
This stores the maximum values seen by a channel.
|
|
| static const bool | channelsInUse [LESENSE_CHANNELS] = LESENSE_CAPSENSE_CH_IN_USE |
|
A bit vector which represents the channels to iterate through.
|
|
| static volatile uint32_t | channelValues [LESENSE_CHANNELS] |
|
This vector stores the latest read values from LESENSE.
|
|
| static volatile uint8_t | currentChannel |
| static void(* | lesenseChCb )(void) |
| static void(* | lesenseScanCb )(void) |
Function Documentation
| void CAPLESENSE_setupCMU | ( | void |
|
) |
Setup the CMU.
Prototypes
Definition at line
84
of file
caplesense.c
.
References CMU_ClockDivSet() , CMU_ClockEnable() , CMU_ClockSelectSet() , cmuClkDiv_1 , cmuClock_ACMP0 , cmuClock_ACMP1 , cmuClock_GPIO , cmuClock_HF , cmuClock_HFPER , cmuClock_LESENSE , cmuClock_LFA , cmuClock_LFB , cmuSelect_Disabled , cmuSelect_HFRCO , cmuSelect_LFRCO , and SystemCoreClockUpdate() .
Referenced by CAPLESENSE_Init() .
Variable Documentation
|
static |
This stores the maximum values seen by a channel.
- Parameters
-
LESENSE_CHANNELSVector of channels.
Definition at line
49
of file
caplesense.c
.
Referenced by CAPLESENSE_getNormalizedVal() , CAPLESENSE_getSliderPosition() , CAPSENSE_getNormalizedVal() , CAPSENSE_getPressed() , CAPSENSE_getSliderPosition() , LESENSE_IRQHandler() , and TIMER0_IRQHandler() .
|
static |
A bit vector which represents the channels to iterate through.
- Parameters
-
LESENSE_CHANNELSVector of channels.
Definition at line
61
of file
caplesense.c
.
Referenced by CAPLESENSE_setupLESENSE() , CAPSENSE_Sense() , and LESENSE_IRQHandler() .
|
static |
This vector stores the latest read values from LESENSE.
- Parameters
-
LESENSE_CHANNELSVector of channels.
Definition at line
37
of file
caplesense.c
.
Referenced by CAPLESENSE_getNormalizedVal() , CAPLESENSE_getSliderPosition() , CAPLESENSE_getVal() , CAPSENSE_getNormalizedVal() , CAPSENSE_getPressed() , CAPSENSE_getSliderPosition() , CAPSENSE_getVal() , LESENSE_IRQHandler() , and TIMER0_IRQHandler() .
|
static |
The current channel we are sensing
Definition at line
79
of file
caplesense.c
.
Referenced by CAPSENSE_Sense() , LESENSE_IRQHandler() , and TIMER0_IRQHandler() .
|
static |
Callback function for LESENSE interrupts.
Definition at line
76
of file
caplesense.c
.
Referenced by CAPLESENSE_setupCallbacks() , and LESENSE_IRQHandler() .
|
static |
Local variablesCallback function for LESENSE interrupts.
Definition at line
74
of file
caplesense.c
.
Referenced by CAPLESENSE_setupCallbacks() , and LESENSE_IRQHandler() .