ACMPEMLIB
Detailed Description
Analog comparator (ACMP) Peripheral API.
The Analog Comparator is used to compare voltage of two analog inputs with a digital output indicating which input voltage is higher. Inputs can either be one of the selectable internal references or from external pins. Response time and current consumption can be configured by altering the current supply to the comparator.
ACMP is available to EM3 and is able to wake up the system when input signals pass a certain threshold. Use ACMP_IntEnable to enable an edge interrupt to use this functionality.
This example shows how to use the
em_acmp.h
API for comparing an input pin to an internal 2.5 V reference voltage.
- Note
- ACMP can also be used to compare two separate input pins.
ACMP also contains specialized hardware for capacitive sensing. This module contains the ACMP_CapsenseInit function to initialize ACMP for capacitive sensing and the ACMP_CapsenseChannelSet function to select the current capsense channel.
For applications that require capacitive sensing it is recommended to use a library, such as cslib, which is provided by Silicon Labs.
This module contains functions to control the ACMP peripheral of Silicon Labs 32-bit MCUs and SoCs.
Data Structures |
|
struct | ACMP_CapsenseInit_TypeDef |
struct | ACMP_Init_TypeDef |
struct | ACMP_VAConfig_TypeDef |
struct | ACMP_VBConfig_TypeDef |
Macros |
|
#define | ACMP_CAPSENSE_INIT_DEFAULT |
#define | ACMP_INIT_DEFAULT |
#define | ACMP_VACONFIG_DEFAULT |
#define | ACMP_VBCONFIG_DEFAULT |
Enumerations |
|
enum |
ACMP_Accuracy_TypeDef
{
acmpAccuracyLow = _ACMP_CTRL_ACCURACY_LOW, acmpAccuracyHigh = _ACMP_CTRL_ACCURACY_HIGH } |
enum |
ACMP_CapsenseResistor_TypeDef
{
acmpResistor0 = _ACMP_INPUTSEL_CSRESSEL_RES0, acmpResistor1 = _ACMP_INPUTSEL_CSRESSEL_RES1, acmpResistor2 = _ACMP_INPUTSEL_CSRESSEL_RES2, acmpResistor3 = _ACMP_INPUTSEL_CSRESSEL_RES3, acmpResistor4 = _ACMP_INPUTSEL_CSRESSEL_RES4, acmpResistor5 = _ACMP_INPUTSEL_CSRESSEL_RES5, acmpResistor6 = _ACMP_INPUTSEL_CSRESSEL_RES6, acmpResistor7 = _ACMP_INPUTSEL_CSRESSEL_RES7 } |
enum |
ACMP_Channel_TypeDef
{
acmpInputAPORT0XCH0 = _ACMP_INPUTSEL_POSSEL_APORT0XCH0, acmpInputAPORT0XCH1 = _ACMP_INPUTSEL_POSSEL_APORT0XCH1, acmpInputAPORT0XCH2 = _ACMP_INPUTSEL_POSSEL_APORT0XCH2, acmpInputAPORT0XCH3 = _ACMP_INPUTSEL_POSSEL_APORT0XCH3, acmpInputAPORT0XCH4 = _ACMP_INPUTSEL_POSSEL_APORT0XCH4, acmpInputAPORT0XCH5 = _ACMP_INPUTSEL_POSSEL_APORT0XCH5, acmpInputAPORT0XCH6 = _ACMP_INPUTSEL_POSSEL_APORT0XCH6, acmpInputAPORT0XCH7 = _ACMP_INPUTSEL_POSSEL_APORT0XCH7, acmpInputAPORT0XCH8 = _ACMP_INPUTSEL_POSSEL_APORT0XCH8, acmpInputAPORT0XCH9 = _ACMP_INPUTSEL_POSSEL_APORT0XCH9, acmpInputAPORT0XCH10 = _ACMP_INPUTSEL_POSSEL_APORT0XCH10, acmpInputAPORT0XCH11 = _ACMP_INPUTSEL_POSSEL_APORT0XCH11, acmpInputAPORT0XCH12 = _ACMP_INPUTSEL_POSSEL_APORT0XCH12, acmpInputAPORT0XCH13 = _ACMP_INPUTSEL_POSSEL_APORT0XCH13, acmpInputAPORT0XCH14 = _ACMP_INPUTSEL_POSSEL_APORT0XCH14, acmpInputAPORT0XCH15 = _ACMP_INPUTSEL_POSSEL_APORT0XCH15, acmpInputAPORT0YCH0 = _ACMP_INPUTSEL_POSSEL_APORT0YCH0, acmpInputAPORT0YCH1 = _ACMP_INPUTSEL_POSSEL_APORT0YCH1, acmpInputAPORT0YCH2 = _ACMP_INPUTSEL_POSSEL_APORT0YCH2, acmpInputAPORT0YCH3 = _ACMP_INPUTSEL_POSSEL_APORT0YCH3, acmpInputAPORT0YCH4 = _ACMP_INPUTSEL_POSSEL_APORT0YCH4, acmpInputAPORT0YCH5 = _ACMP_INPUTSEL_POSSEL_APORT0YCH5, acmpInputAPORT0YCH6 = _ACMP_INPUTSEL_POSSEL_APORT0YCH6, acmpInputAPORT0YCH7 = _ACMP_INPUTSEL_POSSEL_APORT0YCH7, acmpInputAPORT0YCH8 = _ACMP_INPUTSEL_POSSEL_APORT0YCH8, acmpInputAPORT0YCH9 = _ACMP_INPUTSEL_POSSEL_APORT0YCH9, acmpInputAPORT0YCH10 = _ACMP_INPUTSEL_POSSEL_APORT0YCH10, acmpInputAPORT0YCH11 = _ACMP_INPUTSEL_POSSEL_APORT0YCH11, acmpInputAPORT0YCH12 = _ACMP_INPUTSEL_POSSEL_APORT0YCH12, acmpInputAPORT0YCH13 = _ACMP_INPUTSEL_POSSEL_APORT0YCH13, acmpInputAPORT0YCH14 = _ACMP_INPUTSEL_POSSEL_APORT0YCH14, acmpInputAPORT0YCH15 = _ACMP_INPUTSEL_POSSEL_APORT0YCH15, acmpInputAPORT1XCH0 = _ACMP_INPUTSEL_POSSEL_APORT1XCH0, acmpInputAPORT1YCH1 = _ACMP_INPUTSEL_POSSEL_APORT1YCH1, acmpInputAPORT1XCH2 = _ACMP_INPUTSEL_POSSEL_APORT1XCH2, acmpInputAPORT1YCH3 = _ACMP_INPUTSEL_POSSEL_APORT1YCH3, acmpInputAPORT1XCH4 = _ACMP_INPUTSEL_POSSEL_APORT1XCH4, acmpInputAPORT1YCH5 = _ACMP_INPUTSEL_POSSEL_APORT1YCH5, acmpInputAPORT1XCH6 = _ACMP_INPUTSEL_POSSEL_APORT1XCH6, acmpInputAPORT1YCH7 = _ACMP_INPUTSEL_POSSEL_APORT1YCH7, acmpInputAPORT1XCH8 = _ACMP_INPUTSEL_POSSEL_APORT1XCH8, acmpInputAPORT1YCH9 = _ACMP_INPUTSEL_POSSEL_APORT1YCH9, acmpInputAPORT1XCH10 = _ACMP_INPUTSEL_POSSEL_APORT1XCH10, acmpInputAPORT1YCH11 = _ACMP_INPUTSEL_POSSEL_APORT1YCH11, acmpInputAPORT1XCH12 = _ACMP_INPUTSEL_POSSEL_APORT1XCH12, acmpInputAPORT1YCH13 = _ACMP_INPUTSEL_POSSEL_APORT1YCH13, acmpInputAPORT1XCH14 = _ACMP_INPUTSEL_POSSEL_APORT1XCH14, acmpInputAPORT1YCH15 = _ACMP_INPUTSEL_POSSEL_APORT1YCH15, acmpInputAPORT1XCH16 = _ACMP_INPUTSEL_POSSEL_APORT1XCH16, acmpInputAPORT1YCH17 = _ACMP_INPUTSEL_POSSEL_APORT1YCH17, acmpInputAPORT1XCH18 = _ACMP_INPUTSEL_POSSEL_APORT1XCH18, acmpInputAPORT1YCH19 = _ACMP_INPUTSEL_POSSEL_APORT1YCH19, acmpInputAPORT1XCH20 = _ACMP_INPUTSEL_POSSEL_APORT1XCH20, acmpInputAPORT1YCH21 = _ACMP_INPUTSEL_POSSEL_APORT1YCH21, acmpInputAPORT1XCH22 = _ACMP_INPUTSEL_POSSEL_APORT1XCH22, acmpInputAPORT1YCH23 = _ACMP_INPUTSEL_POSSEL_APORT1YCH23, acmpInputAPORT1XCH24 = _ACMP_INPUTSEL_POSSEL_APORT1XCH24, acmpInputAPORT1YCH25 = _ACMP_INPUTSEL_POSSEL_APORT1YCH25, acmpInputAPORT1XCH26 = _ACMP_INPUTSEL_POSSEL_APORT1XCH26, acmpInputAPORT1YCH27 = _ACMP_INPUTSEL_POSSEL_APORT1YCH27, acmpInputAPORT1XCH28 = _ACMP_INPUTSEL_POSSEL_APORT1XCH28, acmpInputAPORT1YCH29 = _ACMP_INPUTSEL_POSSEL_APORT1YCH29, acmpInputAPORT1XCH30 = _ACMP_INPUTSEL_POSSEL_APORT1XCH30, acmpInputAPORT1YCH31 = _ACMP_INPUTSEL_POSSEL_APORT1YCH31, acmpInputAPORT2YCH0 = _ACMP_INPUTSEL_POSSEL_APORT2YCH0, acmpInputAPORT2XCH1 = _ACMP_INPUTSEL_POSSEL_APORT2XCH1, acmpInputAPORT2YCH2 = _ACMP_INPUTSEL_POSSEL_APORT2YCH2, acmpInputAPORT2XCH3 = _ACMP_INPUTSEL_POSSEL_APORT2XCH3, acmpInputAPORT2YCH4 = _ACMP_INPUTSEL_POSSEL_APORT2YCH4, acmpInputAPORT2XCH5 = _ACMP_INPUTSEL_POSSEL_APORT2XCH5, acmpInputAPORT2YCH6 = _ACMP_INPUTSEL_POSSEL_APORT2YCH6, acmpInputAPORT2XCH7 = _ACMP_INPUTSEL_POSSEL_APORT2XCH7, acmpInputAPORT2YCH8 = _ACMP_INPUTSEL_POSSEL_APORT2YCH8, acmpInputAPORT2XCH9 = _ACMP_INPUTSEL_POSSEL_APORT2XCH9, acmpInputAPORT2YCH10 = _ACMP_INPUTSEL_POSSEL_APORT2YCH10, acmpInputAPORT2XCH11 = _ACMP_INPUTSEL_POSSEL_APORT2XCH11, acmpInputAPORT2YCH12 = _ACMP_INPUTSEL_POSSEL_APORT2YCH12, acmpInputAPORT2XCH13 = _ACMP_INPUTSEL_POSSEL_APORT2XCH13, acmpInputAPORT2YCH14 = _ACMP_INPUTSEL_POSSEL_APORT2YCH14, acmpInputAPORT2XCH15 = _ACMP_INPUTSEL_POSSEL_APORT2XCH15, acmpInputAPORT2YCH16 = _ACMP_INPUTSEL_POSSEL_APORT2YCH16, acmpInputAPORT2XCH17 = _ACMP_INPUTSEL_POSSEL_APORT2XCH17, acmpInputAPORT2YCH18 = _ACMP_INPUTSEL_POSSEL_APORT2YCH18, acmpInputAPORT2XCH19 = _ACMP_INPUTSEL_POSSEL_APORT2XCH19, acmpInputAPORT2YCH20 = _ACMP_INPUTSEL_POSSEL_APORT2YCH20, acmpInputAPORT2XCH21 = _ACMP_INPUTSEL_POSSEL_APORT2XCH21, acmpInputAPORT2YCH22 = _ACMP_INPUTSEL_POSSEL_APORT2YCH22, acmpInputAPORT2XCH23 = _ACMP_INPUTSEL_POSSEL_APORT2XCH23, acmpInputAPORT2YCH24 = _ACMP_INPUTSEL_POSSEL_APORT2YCH24, acmpInputAPORT2XCH25 = _ACMP_INPUTSEL_POSSEL_APORT2XCH25, acmpInputAPORT2YCH26 = _ACMP_INPUTSEL_POSSEL_APORT2YCH26, acmpInputAPORT2XCH27 = _ACMP_INPUTSEL_POSSEL_APORT2XCH27, acmpInputAPORT2YCH28 = _ACMP_INPUTSEL_POSSEL_APORT2YCH28, acmpInputAPORT2XCH29 = _ACMP_INPUTSEL_POSSEL_APORT2XCH29, acmpInputAPORT2YCH30 = _ACMP_INPUTSEL_POSSEL_APORT2YCH30, acmpInputAPORT2XCH31 = _ACMP_INPUTSEL_POSSEL_APORT2XCH31, acmpInputAPORT3XCH0 = _ACMP_INPUTSEL_POSSEL_APORT3XCH0, acmpInputAPORT3YCH1 = _ACMP_INPUTSEL_POSSEL_APORT3YCH1, acmpInputAPORT3XCH2 = _ACMP_INPUTSEL_POSSEL_APORT3XCH2, acmpInputAPORT3YCH3 = _ACMP_INPUTSEL_POSSEL_APORT3YCH3, acmpInputAPORT3XCH4 = _ACMP_INPUTSEL_POSSEL_APORT3XCH4, acmpInputAPORT3YCH5 = _ACMP_INPUTSEL_POSSEL_APORT3YCH5, acmpInputAPORT3XCH6 = _ACMP_INPUTSEL_POSSEL_APORT3XCH6, acmpInputAPORT3YCH7 = _ACMP_INPUTSEL_POSSEL_APORT3YCH7, acmpInputAPORT3XCH8 = _ACMP_INPUTSEL_POSSEL_APORT3XCH8, acmpInputAPORT3YCH9 = _ACMP_INPUTSEL_POSSEL_APORT3YCH9, acmpInputAPORT3XCH10 = _ACMP_INPUTSEL_POSSEL_APORT3XCH10, acmpInputAPORT3YCH11 = _ACMP_INPUTSEL_POSSEL_APORT3YCH11, acmpInputAPORT3XCH12 = _ACMP_INPUTSEL_POSSEL_APORT3XCH12, acmpInputAPORT3YCH13 = _ACMP_INPUTSEL_POSSEL_APORT3YCH13, acmpInputAPORT3XCH14 = _ACMP_INPUTSEL_POSSEL_APORT3XCH14, acmpInputAPORT3YCH15 = _ACMP_INPUTSEL_POSSEL_APORT3YCH15, acmpInputAPORT3XCH16 = _ACMP_INPUTSEL_POSSEL_APORT3XCH16, acmpInputAPORT3YCH17 = _ACMP_INPUTSEL_POSSEL_APORT3YCH17, acmpInputAPORT3XCH18 = _ACMP_INPUTSEL_POSSEL_APORT3XCH18, acmpInputAPORT3YCH19 = _ACMP_INPUTSEL_POSSEL_APORT3YCH19, acmpInputAPORT3XCH20 = _ACMP_INPUTSEL_POSSEL_APORT3XCH20, acmpInputAPORT3YCH21 = _ACMP_INPUTSEL_POSSEL_APORT3YCH21, acmpInputAPORT3XCH22 = _ACMP_INPUTSEL_POSSEL_APORT3XCH22, acmpInputAPORT3YCH23 = _ACMP_INPUTSEL_POSSEL_APORT3YCH23, acmpInputAPORT3XCH24 = _ACMP_INPUTSEL_POSSEL_APORT3XCH24, acmpInputAPORT3YCH25 = _ACMP_INPUTSEL_POSSEL_APORT3YCH25, acmpInputAPORT3XCH26 = _ACMP_INPUTSEL_POSSEL_APORT3XCH26, acmpInputAPORT3YCH27 = _ACMP_INPUTSEL_POSSEL_APORT3YCH27, acmpInputAPORT3XCH28 = _ACMP_INPUTSEL_POSSEL_APORT3XCH28, acmpInputAPORT3YCH29 = _ACMP_INPUTSEL_POSSEL_APORT3YCH29, acmpInputAPORT3XCH30 = _ACMP_INPUTSEL_POSSEL_APORT3XCH30, acmpInputAPORT3YCH31 = _ACMP_INPUTSEL_POSSEL_APORT3YCH31, acmpInputAPORT4YCH0 = _ACMP_INPUTSEL_POSSEL_APORT4YCH0, acmpInputAPORT4XCH1 = _ACMP_INPUTSEL_POSSEL_APORT4XCH1, acmpInputAPORT4YCH2 = _ACMP_INPUTSEL_POSSEL_APORT4YCH2, acmpInputAPORT4XCH3 = _ACMP_INPUTSEL_POSSEL_APORT4XCH3, acmpInputAPORT4YCH4 = _ACMP_INPUTSEL_POSSEL_APORT4YCH4, acmpInputAPORT4XCH5 = _ACMP_INPUTSEL_POSSEL_APORT4XCH5, acmpInputAPORT4YCH6 = _ACMP_INPUTSEL_POSSEL_APORT4YCH6, acmpInputAPORT4XCH7 = _ACMP_INPUTSEL_POSSEL_APORT4XCH7, acmpInputAPORT4YCH8 = _ACMP_INPUTSEL_POSSEL_APORT4YCH8, acmpInputAPORT4XCH9 = _ACMP_INPUTSEL_POSSEL_APORT4XCH9, acmpInputAPORT4YCH10 = _ACMP_INPUTSEL_POSSEL_APORT4YCH10, acmpInputAPORT4XCH11 = _ACMP_INPUTSEL_POSSEL_APORT4XCH11, acmpInputAPORT4YCH12 = _ACMP_INPUTSEL_POSSEL_APORT4YCH12, acmpInputAPORT4XCH13 = _ACMP_INPUTSEL_POSSEL_APORT4XCH13, acmpInputAPORT4YCH16 = _ACMP_INPUTSEL_POSSEL_APORT4YCH16, acmpInputAPORT4XCH17 = _ACMP_INPUTSEL_POSSEL_APORT4XCH17, acmpInputAPORT4YCH18 = _ACMP_INPUTSEL_POSSEL_APORT4YCH18, acmpInputAPORT4XCH19 = _ACMP_INPUTSEL_POSSEL_APORT4XCH19, acmpInputAPORT4YCH20 = _ACMP_INPUTSEL_POSSEL_APORT4YCH20, acmpInputAPORT4XCH21 = _ACMP_INPUTSEL_POSSEL_APORT4XCH21, acmpInputAPORT4YCH22 = _ACMP_INPUTSEL_POSSEL_APORT4YCH22, acmpInputAPORT4XCH23 = _ACMP_INPUTSEL_POSSEL_APORT4XCH23, acmpInputAPORT4YCH24 = _ACMP_INPUTSEL_POSSEL_APORT4YCH24, acmpInputAPORT4XCH25 = _ACMP_INPUTSEL_POSSEL_APORT4XCH25, acmpInputAPORT4YCH26 = _ACMP_INPUTSEL_POSSEL_APORT4YCH26, acmpInputAPORT4XCH27 = _ACMP_INPUTSEL_POSSEL_APORT4XCH27, acmpInputAPORT4YCH28 = _ACMP_INPUTSEL_POSSEL_APORT4YCH28, acmpInputAPORT4XCH29 = _ACMP_INPUTSEL_POSSEL_APORT4XCH29, acmpInputAPORT4YCH30 = _ACMP_INPUTSEL_POSSEL_APORT4YCH30, acmpInputAPORT4YCH14 = _ACMP_INPUTSEL_POSSEL_APORT4YCH14, acmpInputAPORT4XCH15 = _ACMP_INPUTSEL_POSSEL_APORT4XCH15, acmpInputAPORT4XCH31 = _ACMP_INPUTSEL_POSSEL_APORT4XCH31, acmpInputDACOUT0 = _ACMP_INPUTSEL_POSSEL_DACOUT0, acmpInputDACOUT1 = _ACMP_INPUTSEL_POSSEL_DACOUT1, acmpInputVLP = _ACMP_INPUTSEL_POSSEL_VLP, acmpInputVBDIV = _ACMP_INPUTSEL_POSSEL_VBDIV, acmpInputVADIV = _ACMP_INPUTSEL_POSSEL_VADIV, acmpInputVDD = _ACMP_INPUTSEL_POSSEL_VDD, acmpInputVSS = _ACMP_INPUTSEL_POSSEL_VSS } |
enum |
ACMP_ExternalInput_Typedef
{
acmpExternalInputAPORT0X = _ACMP_EXTIFCTRL_APORTSEL_APORT0X, acmpExternalInputAPORT0Y = _ACMP_EXTIFCTRL_APORTSEL_APORT0Y, acmpExternalInputAPORT1X = _ACMP_EXTIFCTRL_APORTSEL_APORT1X, acmpExternalInputAPORT1Y = _ACMP_EXTIFCTRL_APORTSEL_APORT1Y, acmpExternalInputAPORT1XY = _ACMP_EXTIFCTRL_APORTSEL_APORT1XY, acmpExternalInputAPORT2X = _ACMP_EXTIFCTRL_APORTSEL_APORT2X, acmpExternalInputAPORT2Y = _ACMP_EXTIFCTRL_APORTSEL_APORT2Y, acmpExternalInputAPORT2YX = _ACMP_EXTIFCTRL_APORTSEL_APORT2YX, acmpExternalInputAPORT3X = _ACMP_EXTIFCTRL_APORTSEL_APORT3X, acmpExternalInputAPORT3Y = _ACMP_EXTIFCTRL_APORTSEL_APORT3Y, acmpExternalInputAPORT3XY = _ACMP_EXTIFCTRL_APORTSEL_APORT3XY, acmpExternalInputAPORT4X = _ACMP_EXTIFCTRL_APORTSEL_APORT4X, acmpExternalInputAPORT4Y = _ACMP_EXTIFCTRL_APORTSEL_APORT4Y, acmpExternalInputAPORT4YX = _ACMP_EXTIFCTRL_APORTSEL_APORT4YX } |
enum |
ACMP_HysteresisLevel_TypeDef
{
acmpHysteresisLevel0 = _ACMP_HYSTERESIS0_HYST_HYST0, acmpHysteresisLevel1 = _ACMP_HYSTERESIS0_HYST_HYST1, acmpHysteresisLevel2 = _ACMP_HYSTERESIS0_HYST_HYST2, acmpHysteresisLevel3 = _ACMP_HYSTERESIS0_HYST_HYST3, acmpHysteresisLevel4 = _ACMP_HYSTERESIS0_HYST_HYST4, acmpHysteresisLevel5 = _ACMP_HYSTERESIS0_HYST_HYST5, acmpHysteresisLevel6 = _ACMP_HYSTERESIS0_HYST_HYST6, acmpHysteresisLevel7 = _ACMP_HYSTERESIS0_HYST_HYST7, acmpHysteresisLevel8 = _ACMP_HYSTERESIS0_HYST_HYST8, acmpHysteresisLevel9 = _ACMP_HYSTERESIS0_HYST_HYST9, acmpHysteresisLevel10 = _ACMP_HYSTERESIS0_HYST_HYST10, acmpHysteresisLevel11 = _ACMP_HYSTERESIS0_HYST_HYST11, acmpHysteresisLevel12 = _ACMP_HYSTERESIS0_HYST_HYST12, acmpHysteresisLevel13 = _ACMP_HYSTERESIS0_HYST_HYST13, acmpHysteresisLevel14 = _ACMP_HYSTERESIS0_HYST_HYST14, acmpHysteresisLevel15 = _ACMP_HYSTERESIS0_HYST_HYST15 } |
enum |
ACMP_InputRange_TypeDef
{
acmpInputRangeFull = _ACMP_CTRL_INPUTRANGE_FULL, acmpInputRangeHigh = _ACMP_CTRL_INPUTRANGE_GTVDDDIV2, acmpInputRangeLow = _ACMP_CTRL_INPUTRANGE_LTVDDDIV2 } |
enum |
ACMP_PowerSource_TypeDef
{
acmpPowerSourceAvdd = _ACMP_CTRL_PWRSEL_AVDD, acmpPowerSourceDvdd = _ACMP_CTRL_PWRSEL_DVDD, acmpPowerSourceIOVdd0 = _ACMP_CTRL_PWRSEL_IOVDD0, acmpPowerSourceIOVdd1 = _ACMP_CTRL_PWRSEL_IOVDD1 } |
enum |
ACMP_VAInput_TypeDef
{
acmpVAInputVDD = _ACMP_INPUTSEL_VASEL_VDD, acmpVAInputAPORT2YCH0 = _ACMP_INPUTSEL_VASEL_APORT2YCH0, acmpVAInputAPORT2YCH2 = _ACMP_INPUTSEL_VASEL_APORT2YCH2, acmpVAInputAPORT2YCH4 = _ACMP_INPUTSEL_VASEL_APORT2YCH4, acmpVAInputAPORT2YCH6 = _ACMP_INPUTSEL_VASEL_APORT2YCH6, acmpVAInputAPORT2YCH8 = _ACMP_INPUTSEL_VASEL_APORT2YCH8, acmpVAInputAPORT2YCH10 = _ACMP_INPUTSEL_VASEL_APORT2YCH10, acmpVAInputAPORT2YCH12 = _ACMP_INPUTSEL_VASEL_APORT2YCH12, acmpVAInputAPORT2YCH14 = _ACMP_INPUTSEL_VASEL_APORT2YCH14, acmpVAInputAPORT2YCH16 = _ACMP_INPUTSEL_VASEL_APORT2YCH16, acmpVAInputAPORT2YCH18 = _ACMP_INPUTSEL_VASEL_APORT2YCH18, acmpVAInputAPORT2YCH20 = _ACMP_INPUTSEL_VASEL_APORT2YCH20, acmpVAInputAPORT2YCH22 = _ACMP_INPUTSEL_VASEL_APORT2YCH22, acmpVAInputAPORT2YCH24 = _ACMP_INPUTSEL_VASEL_APORT2YCH24, acmpVAInputAPORT2YCH26 = _ACMP_INPUTSEL_VASEL_APORT2YCH26, acmpVAInputAPORT2YCH28 = _ACMP_INPUTSEL_VASEL_APORT2YCH28, acmpVAInputAPORT2YCH30 = _ACMP_INPUTSEL_VASEL_APORT2YCH30, acmpVAInputAPORT1XCH0 = _ACMP_INPUTSEL_VASEL_APORT1XCH0, acmpVAInputAPORT1YCH1 = _ACMP_INPUTSEL_VASEL_APORT1YCH1, acmpVAInputAPORT1XCH2 = _ACMP_INPUTSEL_VASEL_APORT1XCH2, acmpVAInputAPORT1YCH3 = _ACMP_INPUTSEL_VASEL_APORT1YCH3, acmpVAInputAPORT1XCH4 = _ACMP_INPUTSEL_VASEL_APORT1XCH4, acmpVAInputAPORT1YCH5 = _ACMP_INPUTSEL_VASEL_APORT1YCH5, acmpVAInputAPORT1XCH6 = _ACMP_INPUTSEL_VASEL_APORT1XCH6, acmpVAInputAPORT1YCH7 = _ACMP_INPUTSEL_VASEL_APORT1YCH7, acmpVAInputAPORT1XCH8 = _ACMP_INPUTSEL_VASEL_APORT1XCH8, acmpVAInputAPORT1YCH9 = _ACMP_INPUTSEL_VASEL_APORT1YCH9, acmpVAInputAPORT1XCH10 = _ACMP_INPUTSEL_VASEL_APORT1XCH10, acmpVAInputAPORT1YCH11 = _ACMP_INPUTSEL_VASEL_APORT1YCH11, acmpVAInputAPORT1XCH12 = _ACMP_INPUTSEL_VASEL_APORT1XCH12, acmpVAInputAPORT1YCH13 = _ACMP_INPUTSEL_VASEL_APORT1YCH13, acmpVAInputAPORT1XCH14 = _ACMP_INPUTSEL_VASEL_APORT1XCH14, acmpVAInputAPORT1YCH15 = _ACMP_INPUTSEL_VASEL_APORT1YCH15, acmpVAInputAPORT1XCH16 = _ACMP_INPUTSEL_VASEL_APORT1XCH16, acmpVAInputAPORT1YCH17 = _ACMP_INPUTSEL_VASEL_APORT1YCH17, acmpVAInputAPORT1XCH18 = _ACMP_INPUTSEL_VASEL_APORT1XCH18, acmpVAInputAPORT1YCH19 = _ACMP_INPUTSEL_VASEL_APORT1YCH19, acmpVAInputAPORT1XCH20 = _ACMP_INPUTSEL_VASEL_APORT1XCH20, acmpVAInputAPORT1YCH21 = _ACMP_INPUTSEL_VASEL_APORT1YCH21, acmpVAInputAPORT1XCH22 = _ACMP_INPUTSEL_VASEL_APORT1XCH22, acmpVAInputAPORT1YCH23 = _ACMP_INPUTSEL_VASEL_APORT1YCH23, acmpVAInputAPORT1XCH24 = _ACMP_INPUTSEL_VASEL_APORT1XCH24, acmpVAInputAPORT1YCH25 = _ACMP_INPUTSEL_VASEL_APORT1YCH25, acmpVAInputAPORT1XCH26 = _ACMP_INPUTSEL_VASEL_APORT1XCH26, acmpVAInputAPORT1YCH27 = _ACMP_INPUTSEL_VASEL_APORT1YCH27, acmpVAInputAPORT1XCH28 = _ACMP_INPUTSEL_VASEL_APORT1XCH28, acmpVAInputAPORT1YCH29 = _ACMP_INPUTSEL_VASEL_APORT1YCH29, acmpVAInputAPORT1XCH30 = _ACMP_INPUTSEL_VASEL_APORT1XCH30, acmpVAInputAPORT1YCH31 = _ACMP_INPUTSEL_VASEL_APORT1YCH31 } |
enum |
ACMP_VBInput_TypeDef
{
acmpVBInput1V25 = _ACMP_INPUTSEL_VBSEL_1V25, acmpVBInput2V5 = _ACMP_INPUTSEL_VBSEL_2V5 } |
enum |
ACMP_VLPInput_Typedef
{
acmpVLPInputVADIV = _ACMP_INPUTSEL_VLPSEL_VADIV, acmpVLPInputVBDIV = _ACMP_INPUTSEL_VLPSEL_VBDIV } |
Functions |
|
void | ACMP_CapsenseChannelSet ( ACMP_TypeDef *acmp, ACMP_Channel_TypeDef channel) |
Set the ACMP channel used for capacitive sensing.
|
|
void | ACMP_CapsenseInit ( ACMP_TypeDef *acmp, const ACMP_CapsenseInit_TypeDef *init) |
Set up ACMP for use in capacitive sense applications.
|
|
void | ACMP_ChannelSet ( ACMP_TypeDef *acmp, ACMP_Channel_TypeDef negSel, ACMP_Channel_TypeDef posSel) |
Set which channels should be used in ACMP comparisons.
|
|
void | ACMP_Disable ( ACMP_TypeDef *acmp) |
Disable ACMP.
|
|
void | ACMP_Enable ( ACMP_TypeDef *acmp) |
Enable ACMP.
|
|
void | ACMP_ExternalInputSelect ( ACMP_TypeDef *acmp, ACMP_ExternalInput_Typedef aport) |
Select and enable external input.
|
|
void | ACMP_GPIOSetup ( ACMP_TypeDef *acmp, uint32_t location, bool enable, bool invert) |
Set up GPIO output from ACMP.
|
|
void | ACMP_Init ( ACMP_TypeDef *acmp, const ACMP_Init_TypeDef *init) |
Initialize ACMP.
|
|
__STATIC_INLINE void | ACMP_IntClear ( ACMP_TypeDef *acmp, uint32_t flags) |
Clear one or more pending ACMP interrupts.
|
|
__STATIC_INLINE void | ACMP_IntDisable ( ACMP_TypeDef *acmp, uint32_t flags) |
Disable one or more ACMP interrupts.
|
|
__STATIC_INLINE void | ACMP_IntEnable ( ACMP_TypeDef *acmp, uint32_t flags) |
Enable one or more ACMP interrupts.
|
|
__STATIC_INLINE uint32_t | ACMP_IntGet ( ACMP_TypeDef *acmp) |
Get pending ACMP interrupt flags.
|
|
__STATIC_INLINE uint32_t | ACMP_IntGetEnabled ( ACMP_TypeDef *acmp) |
Get enabled and pending ACMP interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
|
|
__STATIC_INLINE void | ACMP_IntSet ( ACMP_TypeDef *acmp, uint32_t flags) |
Set one or more pending ACMP interrupts from software.
|
|
void | ACMP_Reset ( ACMP_TypeDef *acmp) |
Reset ACMP to the same state that it was in after a hardware reset.
|
|
void | ACMP_VASetup ( ACMP_TypeDef *acmp, const ACMP_VAConfig_TypeDef *vaconfig) |
Set up the VA source.
|
|
void | ACMP_VBSetup ( ACMP_TypeDef *acmp, const ACMP_VBConfig_TypeDef *vbconfig) |
Set up the VB Source.
|
|
Macro Definition Documentation
#define ACMP_CAPSENSE_INIT_DEFAULT |
A default configuration for capacitive sense mode initialization.
Definition at line
731
of file
em_acmp.h
.
Referenced by CAPSENSE_Init() .
#define ACMP_INIT_DEFAULT |
Default configuration for ACMP regular initialization.
Definition at line
876
of file
em_acmp.h
.
#define ACMP_VACONFIG_DEFAULT |
Definition at line
933
of file
em_acmp.h
.
#define ACMP_VBCONFIG_DEFAULT |
Definition at line
966
of file
em_acmp.h
.
Enumeration Type Documentation
Resistor values used for the internal capacative sense resistor. See data sheet for your device for details on each resistor value.
Definition at line
100
of file
em_acmp.h
.
enum ACMP_Channel_TypeDef |
ACMP Input Selection.
Definition at line
397
of file
em_acmp.h
.
ACMP external input select. This type is used to select which APORT is used by an external module, such as LESENSE, when it's taking control over the ACMP input.
Definition at line
620
of file
em_acmp.h
.
Hysteresis level. See data sheet for your device for details on each level.
Definition at line
125
of file
em_acmp.h
.
ACMP Power source.
Definition at line
212
of file
em_acmp.h
.
enum ACMP_VAInput_TypeDef |
ACMP input to the VA divider. This enumeration is used to select the input for the VA Divider.
Definition at line
241
of file
em_acmp.h
.
enum ACMP_VBInput_TypeDef |
ACMP input to the VB divider. This enumeration is used to select the input for the VB divider.
Definition at line
299
of file
em_acmp.h
.
ACMP Low-Power Input Selection.
Definition at line
309
of file
em_acmp.h
.
Function Documentation
void ACMP_CapsenseChannelSet | ( | ACMP_TypeDef * |
acmp,
|
ACMP_Channel_TypeDef |
channel
|
||
) |
Set the ACMP channel used for capacitive sensing.
- Note
- A basic example of capacitive sensing can be found in the STK BSP (capsense demo).
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. [in] channel
The ACMP channel to use for capacitive sensing (Possel).
Definition at line
210
of file
em_acmp.c
.
References _ACMP_INPUTSEL_POSSEL_MASK , _ACMP_INPUTSEL_POSSEL_SHIFT , BUS_RegMaskedWrite() , and ACMP_TypeDef::INPUTSEL .
Referenced by CAPSENSE_Measure() .
void ACMP_CapsenseInit | ( | ACMP_TypeDef * |
acmp,
|
const ACMP_CapsenseInit_TypeDef * |
init
|
||
) |
Set up ACMP for use in capacitive sense applications.
This function sets up ACMP for use in capacitive sense applications. To use the capacitive sense functionality in the ACMP, use the PRS output of the ACMP module to count the number of oscillations in the capacitive sense circuit (possibly using a TIMER).
- Note
- A basic example of capacitive sensing can be found in the STK BSP (capsense demo).
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. [in] init
A pointer to the initialization structure used to configure ACMP for capacitive sensing operation.
Definition at line
128
of file
em_acmp.c
.
References _ACMP_CTRL_BIASPROG_MASK , _ACMP_CTRL_BIASPROG_SHIFT , _ACMP_CTRL_EN_SHIFT , _ACMP_CTRL_FULLBIAS_SHIFT , _ACMP_CTRL_RESETVALUE , _ACMP_HYSTERESIS0_DIVVA_SHIFT , _ACMP_HYSTERESIS0_HYST_SHIFT , _ACMP_HYSTERESIS1_DIVVA_SHIFT , _ACMP_HYSTERESIS1_HYST_SHIFT , _ACMP_INPUTSEL_CSRESSEL_SHIFT , ACMP_CTRL_ACCURACY_HIGH , ACMP_Disable() , ACMP_Enable() , ACMP_INPUTSEL_CSRESEN , ACMP_INPUTSEL_NEGSEL_VADIV , ACMP_INPUTSEL_VASEL_VDD , ACMP_CapsenseInit_TypeDef::biasProg , BUS_RegBitWrite() , ACMP_TypeDef::CTRL , ACMP_CapsenseInit_TypeDef::enable , ACMP_CapsenseInit_TypeDef::fullBias , ACMP_TypeDef::HYSTERESIS0 , ACMP_TypeDef::HYSTERESIS1 , ACMP_CapsenseInit_TypeDef::hysteresisLevel_0 , ACMP_CapsenseInit_TypeDef::hysteresisLevel_1 , ACMP_TypeDef::INPUTSEL , ACMP_CapsenseInit_TypeDef::resistor , ACMP_CapsenseInit_TypeDef::vddLevelHigh , and ACMP_CapsenseInit_TypeDef::vddLevelLow .
Referenced by CAPLESENSE_setupACMP() , and CAPSENSE_Init() .
void ACMP_ChannelSet | ( | ACMP_TypeDef * |
acmp,
|
ACMP_Channel_TypeDef |
negSel,
|
||
ACMP_Channel_TypeDef |
posSel
|
||
) |
Set which channels should be used in ACMP comparisons.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. negSel
A channel to use on the negative input to the ACMP. posSel
A channel to use on the positive input to the ACMP.
Definition at line
453
of file
em_acmp.c
.
References _ACMP_INPUTSEL_NEGSEL_MASK , _ACMP_INPUTSEL_NEGSEL_SHIFT , _ACMP_INPUTSEL_POSSEL_MASK , _ACMP_INPUTSEL_POSSEL_SHIFT , and ACMP_TypeDef::INPUTSEL .
void ACMP_Disable | ( | ACMP_TypeDef * |
acmp
|
) |
Disable ACMP.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block.
Definition at line
248
of file
em_acmp.c
.
References ACMP_CTRL_EN , and ACMP_TypeDef::CTRL .
Referenced by ACMP_CapsenseInit() , ACMP_Init() , ACMP_Reset() , and CAPSENSE_Sense() .
void ACMP_Enable | ( | ACMP_TypeDef * |
acmp
|
) |
Enable ACMP.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block.
Definition at line
267
of file
em_acmp.c
.
References ACMP_CTRL_EN , and ACMP_TypeDef::CTRL .
Referenced by ACMP_CapsenseInit() , ACMP_Init() , ACMP_Reset() , and CAPSENSE_Sense() .
void ACMP_ExternalInputSelect | ( | ACMP_TypeDef * |
acmp,
|
ACMP_ExternalInput_Typedef |
aport
|
||
) |
Select and enable external input.
This is used when an external module needs to take control of the ACMP POSSEL field to configure the APORT input for the ACMP. Modules, such as LESENSE, use this to change the ACMP input during a scan sequence.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. [in] aport
This parameter decides which APORT(s) the ACMP will use when it's controlled by an external module.
Definition at line
296
of file
em_acmp.c
.
References _ACMP_EXTIFCTRL_APORTSEL_SHIFT , ACMP_EXTIFCTRL_EN , ACMP_STATUS_EXTIFACT , ACMP_TypeDef::EXTIFCTRL , and ACMP_TypeDef::STATUS .
void ACMP_GPIOSetup | ( | ACMP_TypeDef * |
acmp,
|
uint32_t |
location,
|
||
bool |
enable,
|
||
bool |
invert
|
||
) |
Set up GPIO output from ACMP.
- Note
-
GPIO must be enabled in the CMU before this function call, i.e.,
CMU_ClockEnable(cmuClock_GPIO, true);
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. location
The pin location to use. See the data sheet for location to pin mappings. enable
Enable or disable pin output. invert
Invert output.
Definition at line
408
of file
em_acmp.c
.
References _ACMP_CTRL_GPIOINV_MASK , _ACMP_CTRL_GPIOINV_SHIFT , _ACMP_ROUTELOC0_OUTLOC_SHIFT , ACMP_ROUTEPEN_OUTPEN , BUS_RegMaskedWrite() , ACMP_TypeDef::CTRL , ACMP_TypeDef::ROUTELOC0 , and ACMP_TypeDef::ROUTEPEN .
Referenced by CAPLESENSE_setupACMP() .
void ACMP_Init | ( | ACMP_TypeDef * |
acmp,
|
const ACMP_Init_TypeDef * |
init
|
||
) |
Initialize ACMP.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. [in] init
A pointer to the initialization structure used to configure ACMP.
Definition at line
515
of file
em_acmp.c
.
References _ACMP_CTRL_ACCURACY_SHIFT , _ACMP_CTRL_BIASPROG_MASK , _ACMP_CTRL_BIASPROG_SHIFT , _ACMP_CTRL_FULLBIAS_SHIFT , _ACMP_CTRL_IFALL_SHIFT , _ACMP_CTRL_INACTVAL_SHIFT , _ACMP_CTRL_INPUTRANGE_SHIFT , _ACMP_CTRL_IRISE_SHIFT , _ACMP_CTRL_PWRSEL_SHIFT , _ACMP_INPUTSEL_VLPSEL_SHIFT , ACMP_Init_TypeDef::accuracy , ACMP_Disable() , ACMP_Enable() , ACMP_Init_TypeDef::biasProg , BUS_RegMaskedWrite() , ACMP_TypeDef::CTRL , ACMP_Init_TypeDef::enable , ACMP_Init_TypeDef::fullBias , ACMP_TypeDef::HYSTERESIS0 , ACMP_TypeDef::HYSTERESIS1 , ACMP_Init_TypeDef::hysteresisLevel_0 , ACMP_Init_TypeDef::hysteresisLevel_1 , ACMP_Init_TypeDef::inactiveValue , ACMP_Init_TypeDef::inputRange , ACMP_TypeDef::INPUTSEL , ACMP_Init_TypeDef::interruptOnFallingEdge , ACMP_Init_TypeDef::interruptOnRisingEdge , ACMP_Init_TypeDef::powerSource , and ACMP_Init_TypeDef::vlpInput .
__STATIC_INLINE void ACMP_IntClear | ( | ACMP_TypeDef * |
acmp,
|
uint32_t |
flags
|
||
) |
Clear one or more pending ACMP interrupts.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. [in] flags
Pending ACMP interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IFC_EDGE or ACMP_IFC_WARMUP .
Definition at line
1012
of file
em_acmp.h
.
References ACMP_TypeDef::IFC .
__STATIC_INLINE void ACMP_IntDisable | ( | ACMP_TypeDef * |
acmp,
|
uint32_t |
flags
|
||
) |
Disable one or more ACMP interrupts.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. [in] flags
ACMP interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IEN_EDGE or ACMP_IEN_WARMUP .
Definition at line
1033
of file
em_acmp.h
.
References BUS_RegMaskedClear() , and ACMP_TypeDef::IEN .
__STATIC_INLINE void ACMP_IntEnable | ( | ACMP_TypeDef * |
acmp,
|
uint32_t |
flags
|
||
) |
Enable one or more ACMP interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using ACMP_IntClear() prior to enabling if a pending interrupt should be ignored.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. [in] flags
ACMP interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IEN_EDGE or ACMP_IEN_WARMUP .
Definition at line
1055
of file
em_acmp.h
.
References ACMP_TypeDef::IEN .
__STATIC_INLINE uint32_t ACMP_IntGet | ( | ACMP_TypeDef * |
acmp
|
) |
Get pending ACMP interrupt flags.
- Note
- This function does not clear event bits.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block.
- Returns
- Pending ACMP interrupt sources. A bitwise logic OR combination of valid interrupt flags for the ACMP module. The pending interrupt sources can be, for instance, ACMP_IF_EDGE or ACMP_IF_WARMUP .
Definition at line
1079
of file
em_acmp.h
.
References ACMP_TypeDef::IF .
__STATIC_INLINE uint32_t ACMP_IntGetEnabled | ( | ACMP_TypeDef * |
acmp
|
) |
Get enabled and pending ACMP interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block.
- Note
- This function does not clear interrupt flags.
- Returns
-
Pending and enabled ACMP interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in ACMPx_IEN_nnn register (ACMPx_IEN_nnn) and
- the OR combination of valid interrupt flags of the ACMP module (ACMPx_IF_nnn).
Definition at line
1103
of file
em_acmp.h
.
References ACMP_TypeDef::IEN , and ACMP_TypeDef::IF .
__STATIC_INLINE void ACMP_IntSet | ( | ACMP_TypeDef * |
acmp,
|
uint32_t |
flags
|
||
) |
Set one or more pending ACMP interrupts from software.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. [in] flags
ACMP interrupt sources to set as pending. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IFS_EDGE or ACMP_IFS_WARMUP .
Definition at line
1127
of file
em_acmp.h
.
References ACMP_TypeDef::IFS .
void ACMP_Reset | ( | ACMP_TypeDef * |
acmp
|
) |
Reset ACMP to the same state that it was in after a hardware reset.
- Note
- The GPIO ACMP ROUTE register is NOT reset by this function to allow for centralized setup of this feature.
- The peripheral may be enabled and disabled during reset.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block.
Definition at line
319
of file
em_acmp.c
.
References _ACMP_CTRL_RESETVALUE , _ACMP_HYSTERESIS0_RESETVALUE , _ACMP_HYSTERESIS1_RESETVALUE , _ACMP_IEN_RESETVALUE , _ACMP_IF_MASK , _ACMP_INPUTSEL_RESETVALUE , ACMP_Disable() , ACMP_Enable() , ACMP_TypeDef::CTRL , ACMP_TypeDef::HYSTERESIS0 , ACMP_TypeDef::HYSTERESIS1 , ACMP_TypeDef::IEN , ACMP_TypeDef::IFC , and ACMP_TypeDef::INPUTSEL .
void ACMP_VASetup | ( | ACMP_TypeDef * |
acmp,
|
const ACMP_VAConfig_TypeDef * |
vaconfig
|
||
) |
Set up the VA source.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. [in] vaconfig
A pointer to the structure used to configure the VA source. This structure contains the input source and the 2 divider values.
Definition at line
591
of file
em_acmp.c
.
References _ACMP_HYSTERESIS0_DIVVA_MASK , _ACMP_HYSTERESIS0_DIVVA_SHIFT , _ACMP_HYSTERESIS1_DIVVA_MASK , _ACMP_HYSTERESIS1_DIVVA_SHIFT , _ACMP_INPUTSEL_VASEL_MASK , _ACMP_INPUTSEL_VASEL_SHIFT , BUS_RegMaskedWrite() , ACMP_VAConfig_TypeDef::div0 , ACMP_VAConfig_TypeDef::div1 , ACMP_TypeDef::HYSTERESIS0 , ACMP_TypeDef::HYSTERESIS1 , ACMP_VAConfig_TypeDef::input , and ACMP_TypeDef::INPUTSEL .
void ACMP_VBSetup | ( | ACMP_TypeDef * |
acmp,
|
const ACMP_VBConfig_TypeDef * |
vbconfig
|
||
) |
Set up the VB Source.
- Parameters
-
[in] acmp
A pointer to the ACMP peripheral register block. [in] vbconfig
A pointer to the structure used to configure the VB source. This structure contains the input source and the 2 divider values.
Definition at line
617
of file
em_acmp.c
.
References _ACMP_HYSTERESIS0_DIVVB_MASK , _ACMP_HYSTERESIS0_DIVVB_SHIFT , _ACMP_HYSTERESIS1_DIVVB_MASK , _ACMP_HYSTERESIS1_DIVVB_SHIFT , _ACMP_INPUTSEL_VBSEL_MASK , _ACMP_INPUTSEL_VBSEL_SHIFT , BUS_RegMaskedWrite() , ACMP_VBConfig_TypeDef::div0 , ACMP_VBConfig_TypeDef::div1 , ACMP_TypeDef::HYSTERESIS0 , ACMP_TypeDef::HYSTERESIS1 , ACMP_VBConfig_TypeDef::input , and ACMP_TypeDef::INPUTSEL .