NorFlashKit Drivers
Data Structures | |
struct | NORFLASH_Info_TypeDef |
NORFLASH device information struct. | |
Enumerations | |
enum | NORFLASH_Status_TypeDef { NORFLASH_STATUS_OK = 0, NORFLASH_NONUNIFORM_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6, NORFLASH_STATUS_OK = 0, NORFLASH_UNSUPPORTED_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6 } |
NORFLASH status enumerator. | |
enum | NORFLASH_Status_TypeDef { NORFLASH_STATUS_OK = 0, NORFLASH_NONUNIFORM_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6, NORFLASH_STATUS_OK = 0, NORFLASH_UNSUPPORTED_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6 } |
NORFLASH status enumerator. | |
Functions | |
bool | NORFLASH_AddressValid (uint32_t addr) |
Check if an address is valid for the flash device. | |
NORFLASH_Info_TypeDef * | NORFLASH_DeviceInfo (void) |
Return a pointer to a NORFLASH_Info_TypeDef, which contain vital flash device information. | |
int | NORFLASH_EraseDevice (void) |
Erase entire flash device. | |
int | NORFLASH_EraseSector (uint32_t addr) |
Erase a sector in the flash device. | |
uint32_t | NORFLASH_getDeviceID (void) |
Get flash device ID. | |
uint32_t | NORFLASH_getDeviceSize (void) |
Get flash device size. | |
uint32_t | NORFLASH_getSectorRegionCount (void) |
Get flash sector region count. | |
uint32_t | NORFLASH_getVendorID (void) |
Get manufacturer ID. | |
int | NORFLASH_Init (void) |
Initialize the NORFLASH module. | |
int | NORFLASH_Program (uint32_t addr, uint8_t *data, uint32_t count) |
Program the flash device. | |
int | NORFLASH_ProgramByte (uint32_t addr, uint8_t data) |
Program a single byte in the flash device. | |
int | NORFLASH_ProgramWord16 (uint32_t addr, uint16_t data) |
Program a word (16bit) in the flash device. | |
int | NORFLASH_ProgramWord32 (uint32_t addr, uint32_t data) |
Program a word (32bit) in the flash device. | |
Enumeration Type Documentation
NORFLASH status enumerator.
Definition at line 38
of file norflash.h
.
NORFLASH status enumerator.
Definition at line 38
of file norflash_s29gl.h
.
Function Documentation
bool NORFLASH_AddressValid | ( | uint32_t | addr | ) |
Check if an address is valid for the flash device.
- Parameters
-
[in] addr
The address value to check.
- Returns
- True if address value is valid, false otherwise.
Definition at line 48
of file norflash.c
.
References NORFLASH_Info_TypeDef::baseAddress, NORFLASH_Info_TypeDef::deviceSize, and NORFLASH_STATUS_OK.
Referenced by NORFLASH_EraseSector(), NORFLASH_Program(), and NORFLASH_ProgramWord16().
NORFLASH_Info_TypeDef* NORFLASH_DeviceInfo | ( | void |
| ) |
Return a pointer to a NORFLASH_Info_TypeDef, which contain vital flash device information.
- Returns
- NULL if unable to initialize the flash if no prior call to NORFLASH_Init() has been made. Pointer to a NORFLASH_Info_TypeDef on success.
Definition at line 74
of file norflash.c
.
References NORFLASH_STATUS_OK.
int NORFLASH_EraseDevice | ( | void |
| ) |
Erase entire flash device.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line 93
of file norflash.c
.
References NORFLASH_Info_TypeDef::baseAddress, and NORFLASH_STATUS_OK.
int NORFLASH_EraseSector | ( | uint32_t | addr | ) |
Erase a sector in the flash device.
- Parameters
-
[in] addr
Address of the sector to erase.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line 126
of file norflash.c
.
References NORFLASH_AddressValid(), NORFLASH_INVALID_ADDRESS, NORFLASH_STATUS_OK, and NORFLASH_Info_TypeDef::sectorSize.
uint32_t NORFLASH_getDeviceID | ( | void |
| ) |
Get flash device ID.
- Returns
- Flash device ID
Definition at line 409
of file norflash_s29gl.c
.
uint32_t NORFLASH_getDeviceSize | ( | void |
| ) |
Get flash device size.
- Returns
- Flash device size
Definition at line 427
of file norflash_s29gl.c
.
uint32_t NORFLASH_getSectorRegionCount | ( | void |
| ) |
Get flash sector region count.
- Returns
- Flash sector region
Definition at line 439
of file norflash_s29gl.c
.
uint32_t NORFLASH_getVendorID | ( | void |
| ) |
Get manufacturer ID.
- Returns
- Manufacturer ID
Definition at line 397
of file norflash_s29gl.c
.
int NORFLASH_Init | ( | void |
| ) |
Initialize the NORFLASH module.
- Note
- This function should be called before any other NORFLASH_xxx() functions are used.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line 169
of file norflash.c
.
int NORFLASH_Program | ( | uint32_t | addr, |
uint8_t * | data, |
||
uint32_t | count |
||
) |
Program the flash device.
- Note
- It is assumed that the area to be programmed is erased.
- Parameters
-
[in] addr
The first address in the flash to be programmed. [in] data
Pointer to the data to be programmed. [in] count
Number of bytes to be programmed.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line 194
of file norflash.c
.
References NORFLASH_AddressValid(), NORFLASH_INVALID_ADDRESS, NORFLASH_ProgramByte(), NORFLASH_ProgramWord16(), NORFLASH_STATUS_OK, NORFLASH_Info_TypeDef::sectorSize, and SL_MIN.
int NORFLASH_ProgramByte | ( | uint32_t | addr, |
uint8_t | data |
||
) |
Program a single byte in the flash device.
- Note
- It is assumed that the area to be programmed is erased.
- Parameters
-
[in] addr
The address to be programmed. [in] data
The byte value to be programmed.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line 282
of file norflash.c
.
References NORFLASH_ProgramWord16().
Referenced by NORFLASH_Program().
int NORFLASH_ProgramWord16 | ( | uint32_t | addr, |
uint16_t | data |
||
) |
Program a word (16bit) in the flash device.
- Note
- It is assumed that the area to be programmed is erased.
- Parameters
-
[in] addr
The address to be programmed. [in] data
The word value to be programmed.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line 313
of file norflash.c
.
References NORFLASH_AddressValid(), NORFLASH_INVALID_ADDRESS, NORFLASH_MISALIGNED_ADDRESS, and NORFLASH_STATUS_OK.
Referenced by NORFLASH_Program(), NORFLASH_ProgramByte(), and NORFLASH_ProgramWord32().
int NORFLASH_ProgramWord32 | ( | uint32_t | addr, |
uint32_t | data |
||
) |
Program a word (32bit) in the flash device.
- Note
- It is assumed that the area to be programmed is erased.
- Parameters
-
[in] addr
The address to be programmed. [in] data
The word value to be programmed.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line 360
of file norflash.c
.
References NORFLASH_MISALIGNED_ADDRESS, NORFLASH_ProgramWord16(), and NORFLASH_STATUS_OK.