MTB_TypeDef Struct ReferenceDevices > MTB
MTB Register Declaration
Definition at line 49
of file efm32tg11b_mtb.h
.
#include <
efm32tg11b_mtb.h
>
Data Fields | |
__IOM uint32_t | BASE |
__IOM uint32_t | FLOW |
__IOM uint32_t | MASTER |
__IOM uint32_t | POSITION |
Field Documentation
__IOM uint32_t MTB_TypeDef::BASE |
MTB Trace Base Register
Definition at line 53
of file efm32tg11b_mtb.h
.
__IOM uint32_t MTB_TypeDef::FLOW |
MTB Trace Flow Register
Definition at line 52
of file efm32tg11b_mtb.h
.
__IOM uint32_t MTB_TypeDef::MASTER |
MTB Trace Control Register
Definition at line 51
of file efm32tg11b_mtb.h
.
__IOM uint32_t MTB_TypeDef::POSITION |
MTB Trace Position Register.
Definition at line 50
of file efm32tg11b_mtb.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG11B/Include/
efm32tg11b_mtb.h