Unmod_Carrier_PluginEMDRV > EZRADIODRV > Plugin_System

Detailed Description

Unmodulated Carrier plugin, see Plugin System Layer for detailed documentation.


     

.

Data Structures

struct EZRADIODRV_UnmodCarrierHandle
EzRadio unmodulated carrier plug-in instance initialization and handler structure.

Macros

#define EZRADIODRV_UNMOD_CARRIER_PLUGIN_INIT_DEFAULT
Configuration data for EzRadio unmodulated carrier plug-in.

Typedefs

typedef struct EZRADIODRV_UnmodCarrierHandle EZRADIODRV_UnmodCarrierHandle_t
EzRadio unmodulated carrier plug-in instance initialization and handler structure.

Functions

Ecode_t ezradioStartUnmodulatedCarrier ( EZRADIODRV_Handle_t radioHandle)
Starts unmodulated carrier transmission with the radio configurations from the radioHandle parameter.
Ecode_t ezradioStopUnmodulatedCarrier (void)
Stops unmodulated carrier transmission.

Macro Definition Documentation

#define EZRADIODRV_UNMOD_CARRIER_PLUGIN_INIT_DEFAULT
Value:
{ /* Unmodulated Carrier */ \
0, /* Channel */ \
},

Configuration data for EzRadio unmodulated carrier plug-in.

Definition at line 73 of file ezradio_unmod_carrier_plugin.h .

Function Documentation

Ecode_t ezradioStartUnmodulatedCarrier ( EZRADIODRV_Handle_t radioHandle )

Starts unmodulated carrier transmission with the radio configurations from the radioHandle parameter.

Parameters
radioHandle Handler of the EzRadio driver instance where channel configuration is set.
Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 56 of file ezradio_unmod_carrier_plugin.c .

References EZRADIODRV_UnmodCarrierHandle::channel , ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED , ezradio_get_int_status() , ezradio_request_device_state() , ezradio_start_tx() , and EZRADIODRV_HandleData::unmodCarrier .

Ecode_t ezradioStopUnmodulatedCarrier ( void )

Stops unmodulated carrier transmission.

Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 87 of file ezradio_unmod_carrier_plugin.c .

References ECODE_EMDRV_EZRADIODRV_OK , and ezradio_change_state() .