LESENSE_BUF_TypeDef Struct ReferenceDevicesDevices > | LESENSE

LESENSE_BUF LESENSE BUF Register


      

.

Definition at line 47 of file efr32bg12p_lesense_buf.h .

#include < efr32bg12p_lesense_buf.h >

Data Fields

__IOM uint32_t DATA

Field Documentation

__IOM uint32_t LESENSE_BUF_TypeDef::DATA

Scan Results

Definition at line 48 of file efr32bg12p_lesense_buf.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG12P/Include/ efr32bg12p_lesense_buf.h