NORFLASH_Info_TypeDef Struct ReferenceKit Drivers > NorFlash
NORFLASH device information struct.
Definition at line
49
of file
norflash.h
.
#include <
norflash.h
>
Data Fields |
|
| uint32_t | baseAddress |
| uint32_t | deviceId |
| uint32_t | deviceSize |
| uint16_t | manufacturerId |
| uint32_t | sectorCount |
| uint32_t | sectorSize |
Field Documentation
| uint32_t NORFLASH_Info_TypeDef::baseAddress |
The device base address in cpu memory map.
Definition at line
50
of file
norflash.h
.
Referenced by NORFLASH_AddressValid() , and NORFLASH_EraseDevice() .
| uint32_t NORFLASH_Info_TypeDef::deviceId |
The device ID.
Definition at line
51
of file
norflash.h
.
| uint32_t NORFLASH_Info_TypeDef::deviceSize |
Total device size in bytes.
Definition at line
52
of file
norflash.h
.
Referenced by NORFLASH_AddressValid() .
| uint16_t NORFLASH_Info_TypeDef::manufacturerId |
The device manufacturer ID.
Definition at line
55
of file
norflash.h
.
| uint32_t NORFLASH_Info_TypeDef::sectorCount |
Number of sectors in the device.
Definition at line
53
of file
norflash.h
.
| uint32_t NORFLASH_Info_TypeDef::sectorSize |
Sector size in bytes.
Definition at line
54
of file
norflash.h
.
Referenced by NORFLASH_EraseSector() , and NORFLASH_Program() .
The documentation for this struct was generated from the following files:
-
C:/repos/embsw_super_h1/hardware/kit/common/drivers/
norflash.h -
C:/repos/embsw_super_h1/hardware/kit/common/drivers/
norflash_s29gl.h