VDAC_Init_TypeDef Struct ReferenceEMLIB > VDAC
VDAC initialization structure, common for both channels.
Definition at line
160
of file
em_vdac.h
.
#include <
em_vdac.h
>
Data Fields |
|
bool | asyncClockMode |
bool | ch0ResetPre |
bool | diff |
bool | mainCalibration |
bool | outEnablePRS |
uint32_t | prescaler |
VDAC_Ref_TypeDef | reference |
VDAC_Refresh_TypeDef | refresh |
bool | sineEnable |
bool | warmupKeepOn |
Field Documentation
bool VDAC_Init_TypeDef::asyncClockMode |
Selects clock from asynchronous or synchronous (with respect to peripheral clock) source.
Definition at line
166
of file
em_vdac.h
.
Referenced by VDAC_Init() .
bool VDAC_Init_TypeDef::ch0ResetPre |
Enable/disable reset of prescaler on CH 0 start.
Definition at line
181
of file
em_vdac.h
.
Referenced by VDAC_Init() .
bool VDAC_Init_TypeDef::diff |
Select if single ended or differential output mode.
Definition at line
190
of file
em_vdac.h
.
Referenced by VDAC_Init() .
bool VDAC_Init_TypeDef::mainCalibration |
Selects between main and alternate output path calibration values.
Definition at line
162
of file
em_vdac.h
.
Referenced by VDAC_Init() .
bool VDAC_Init_TypeDef::outEnablePRS |
Enable/disable output enable control by CH1 PRS signal.
Definition at line
184
of file
em_vdac.h
.
Referenced by VDAC_Init() .
uint32_t VDAC_Init_TypeDef::prescaler |
Prescaler for VDAC clock. Clock is source clock divided by prescaler+1.
Definition at line
175
of file
em_vdac.h
.
Referenced by VDAC_Init() .
VDAC_Ref_TypeDef VDAC_Init_TypeDef::reference |
VDAC_Refresh_TypeDef VDAC_Init_TypeDef::refresh |
bool VDAC_Init_TypeDef::sineEnable |
bool VDAC_Init_TypeDef::warmupKeepOn |
Warm-up mode, keep VDAC on (in idle) - or shutdown between conversions.
Definition at line
169
of file
em_vdac.h
.
Referenced by VDAC_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_vdac.h