LDMA_CH_TypeDef Struct ReferenceDevicesDevices > | LDMA
LDMA_CH LDMA CH Register
.
Definition at line
47
of file
efr32bg12p_ldma_ch.h
.
#include <
efr32bg12p_ldma_ch.h
>
Data Fields |
|
| __IOM uint32_t | CFG |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | DST |
| __IOM uint32_t | LINK |
| __IOM uint32_t | LOOP |
| __IOM uint32_t | REQSEL |
| uint32_t | RESERVED0 [5U] |
| __IOM uint32_t | SRC |
Field Documentation
| __IOM uint32_t LDMA_CH_TypeDef::CFG |
Channel Configuration Register
Definition at line
49
of file
efr32bg12p_ldma_ch.h
.
| __IOM uint32_t LDMA_CH_TypeDef::CTRL |
Channel Descriptor Control Word Register
Definition at line
51
of file
efr32bg12p_ldma_ch.h
.
| __IOM uint32_t LDMA_CH_TypeDef::DST |
Channel Descriptor Destination Data Address Register
Definition at line
53
of file
efr32bg12p_ldma_ch.h
.
| __IOM uint32_t LDMA_CH_TypeDef::LINK |
Channel Descriptor Link Structure Address Register
Definition at line
54
of file
efr32bg12p_ldma_ch.h
.
| __IOM uint32_t LDMA_CH_TypeDef::LOOP |
Channel Loop Counter Register
Definition at line
50
of file
efr32bg12p_ldma_ch.h
.
| __IOM uint32_t LDMA_CH_TypeDef::REQSEL |
Channel Peripheral Request Select Register
Definition at line
48
of file
efr32bg12p_ldma_ch.h
.
| uint32_t LDMA_CH_TypeDef::RESERVED0[5U] |
Reserved future
Definition at line
55
of file
efr32bg12p_ldma_ch.h
.
| __IOM uint32_t LDMA_CH_TypeDef::SRC |
Channel Descriptor Source Data Address Register
Definition at line
52
of file
efr32bg12p_ldma_ch.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG12P/Include/
efr32bg12p_ldma_ch.h