MSDBOT_CSW_TypeDef Struct ReferenceKit Drivers > Msd
Bulk Only Transport (BOT) Command Status Wrapper (CSW) typedef.
Definition at line 85
of file msdbot.h
.
#include <
msdbot.h
>
Data Fields | |
uint8_t | bCSWStatus |
uint32_t | dCSWDataResidue |
uint32_t | dCSWSignature |
uint32_t | dCSWTag |
Field Documentation
uint8_t MSDBOT_CSW_TypeDef::bCSWStatus |
uint32_t MSDBOT_CSW_TypeDef::dCSWDataResidue |
BOT transfer residue count.
Definition at line 88
of file msdbot.h
.
uint32_t MSDBOT_CSW_TypeDef::dCSWSignature |
The CSW signature (ascii USBS).
Definition at line 86
of file msdbot.h
.
uint32_t MSDBOT_CSW_TypeDef::dCSWTag |
The CSW tag.
Definition at line 87
of file msdbot.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/hardware/kit/common/drivers/
msdbot.h