Components

Software Components

These are some of the RAIL software components available for application use.

Libraries

RAIL library software components provide the ability to choose support for single or multiple protocols. Current components include:

Utilities

Radio utility software components provide optional source code that aid with radio setup and functionality. Current components include:

RAILtest Application

RAILtest application software components are specific to the RAILtest application. Current components include:

RAIL Library Angle of Arrival/Departure (AoX) Utility Antenna Diversity Utility Built-in PHYs for alternate HFXO frequencies Callbacks Utility Coexistence Utility Direct Memory Access (DMA) Utility Energy Friendly Front End Module (EFF) Utility Front End Module (FEM) Utility Initialization Utility Packet Trace Interface (PTI) Utility Power Amplifier (PA) Utility Protocol Utility Recommended Utility RF Path Utility Received Signal Strength Indicator (RSSI) Utility RAILtest Application Core RAILtest Application Graphics