RAIL_DirectModeConfig_t Struct Reference
Chip-specific type that allows the user to specify direct mode parameters using RAIL_ConfigDirectMode() .
#include <
rail_chip_specific.h
>
Data Fields |
|
| bool | syncRx |
|
Enable synchronous RX DOUT using DCLK vs.
|
|
| bool | syncTx |
|
Enable synchronous TX DIN using DCLK vs.
|
|
| uint8_t | doutPort |
|
Only used with directRx.
|
|
| uint8_t | doutPin |
|
Data output (DOUT) GPIO pin.
|
|
| uint8_t | dclkPort |
|
Only used in synchronous mode.
|
|
| uint8_t | dclkPin |
|
Data clock (DCLK) GPIO pin.
|
|
| uint8_t | dinPort |
|
Only used with directTx.
|
|
| uint8_t | dinPin |
|
Data frame (DIN) GPIO pin.
|
|
| uint8_t | doutLoc |
|
Data output (DOUT) location for pin/port.
|
|
| uint8_t | dclkLoc |
|
Data clock (DCLK) location for pin/port.
|
|
| uint8_t | dinLoc |
|
Data frame (DIN) location for pin/port.
|
|
Chip-specific type that allows the user to specify direct mode parameters using RAIL_ConfigDirectMode() .
Definition at line
598
of file
rail_chip_specific.h
.
Field Documentation
◆ dclkLoc
| uint8_t RAIL_DirectModeConfig_t::dclkLoc |
Data clock (DCLK) location for pin/port.
Definition at line
625
of file
rail_chip_specific.h
.
◆ dclkPin
| uint8_t RAIL_DirectModeConfig_t::dclkPin |
Data clock (DCLK) GPIO pin.
Only used in synchronous mode
Definition at line
614
of file
rail_chip_specific.h
.
◆ dclkPort
| uint8_t RAIL_DirectModeConfig_t::dclkPort |
Only used in synchronous mode.
Data clock (DCLK) GPIO port. Only used in synchronous mode
Definition at line
612
of file
rail_chip_specific.h
.
◆ dinLoc
| uint8_t RAIL_DirectModeConfig_t::dinLoc |
Data frame (DIN) location for pin/port.
Definition at line
627
of file
rail_chip_specific.h
.
◆ dinPort
| uint8_t RAIL_DirectModeConfig_t::dinPort |
Only used with directTx.
Data frame (DIN) GPIO port
Definition at line
618
of file
rail_chip_specific.h
.
◆ doutLoc
| uint8_t RAIL_DirectModeConfig_t::doutLoc |
Data output (DOUT) location for pin/port.
Definition at line
623
of file
rail_chip_specific.h
.
◆ doutPort
| uint8_t RAIL_DirectModeConfig_t::doutPort |
Only used with directRx.
Data output (DOUT) GPIO port
Definition at line
606
of file
rail_chip_specific.h
.
◆ syncRx
| bool RAIL_DirectModeConfig_t::syncRx |
Enable synchronous RX DOUT using DCLK vs.
asynchronous RX DOUT.
Definition at line
600
of file
rail_chip_specific.h
.
◆ syncTx
| bool RAIL_DirectModeConfig_t::syncTx |
Enable synchronous TX DIN using DCLK vs.
asynchronous TX DIN.
Definition at line
602
of file
rail_chip_specific.h
.
The documentation for this struct was generated from the following file:
-
chip/efr32/efr32xg1x/
rail_chip_specific.h