RAIL configuration structure.
#include <
rail_chip_specific.h
>
Data Fields | |
void(* | eventsCallback )(RAIL_Handle_t railHandle, RAIL_Events_t events) |
A pointer to a function, which is called whenever a RAIL event occurs. | |
void * | protocol |
Provided for backwards compatibility. | |
RAILSched_Config_t * | scheduler |
Provided for backwards compatibility. | |
RAIL_StateBuffer_t | buffer |
Provided for backwards compatibility. |
RAIL configuration structure.
Definition at line 131
of file rail_chip_specific.h
.
Field Documentation
◆ buffer
RAIL_StateBuffer_t RAIL_Config_t::buffer |
Provided for backwards compatibility.
Ignored.
Definition at line 152
of file rail_chip_specific.h
.
◆ eventsCallback
void(* RAIL_Config_t::eventsCallback) (RAIL_Handle_t railHandle, RAIL_Events_t events) |
A pointer to a function, which is called whenever a RAIL event occurs.
- Parameters
-
[in] railHandle
A handle for a RAIL instance. [in] events
A bit mask of RAIL events.
See the RAIL_Events_t documentation for the list of RAIL events.
Definition at line 140
of file rail_chip_specific.h
.
◆ protocol
void* RAIL_Config_t::protocol |
Provided for backwards compatibility.
Ignored.
Definition at line 144
of file rail_chip_specific.h
.
◆ scheduler
RAILSched_Config_t* RAIL_Config_t::scheduler |
Provided for backwards compatibility.
Ignored.
Definition at line 148
of file rail_chip_specific.h
.
The documentation for this struct was generated from the following file:
- chip/efr32/efr32xg1x/
rail_chip_specific.h