RAIL_RxDutyCycleConfig_t Struct Reference
Structure to configure duty cycled receive mode.
#include <
rail_types.h
>
Data Fields |
|
| RAIL_RxChannelHoppingMode_t | mode |
|
The mode by which RAIL determines when to exit RX.
|
|
| RAIL_RxChannelHoppingParameter_t | parameter |
|
Depending on the 'mode' parameter that was specified, this member is used to parameterize that mode.
|
|
| uint32_t | delay |
|
Idle time in microseconds to wait before re-entering RX.
|
|
| RAIL_RxChannelHoppingDelayMode_t | delayMode |
|
Indicate how the timing specified in 'delay' should be applied.
|
|
| RAIL_RxChannelHoppingOptions_t | options |
|
Bitmask of various options that can be applied to the current duty cycle operation when the mode is >=
RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL_WITH_OPTIONS
(ignored otherwise).
|
|
| int8_t | rssiThresholdDbm |
|
The RSSI threshold (in dBm) below which Rx will end in any mode when
RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD
is specified.
|
|
| uint8_t | reserved2 [1] |
|
Pad bytes reserved for future use and currently ignored.
|
|
Structure to configure duty cycled receive mode.
Definition at line
4131
of file
rail_types.h
.
Field Documentation
◆ mode
| RAIL_RxChannelHoppingMode_t RAIL_RxDutyCycleConfig_t::mode |
The mode by which RAIL determines when to exit RX.
Definition at line
4133
of file
rail_types.h
.
◆ parameter
| RAIL_RxChannelHoppingParameter_t RAIL_RxDutyCycleConfig_t::parameter |
Depending on the 'mode' parameter that was specified, this member is used to parameterize that mode.
See the comments on each value of RAIL_RxChannelHoppingMode_t to learn what to specify here.
Definition at line
4140
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h