Contains RAIL Library Version Information.
#include <
rail_types.h
>
Data Fields | |
uint32_t | hash |
Git hash. | |
uint8_t | major |
Major number. | |
uint8_t | minor |
Minor number. | |
uint8_t | rev |
Revision number. | |
uint8_t | build |
Build number. | |
uint8_t | flags |
Build flags. | |
bool | multiprotocol |
Boolean to indicate whether this is a multiprotocol library or not. |
Contains RAIL Library Version Information.
It is filled in by RAIL_GetVersion().
Definition at line 82
of file rail_types.h
.
Field Documentation
◆ multiprotocol
bool RAIL_Version_t::multiprotocol |
Boolean to indicate whether this is a multiprotocol library or not.
Definition at line 90
of file rail_types.h
.
The documentation for this struct was generated from the following file:
- common/
rail_types.h