RAIL_BLE_TxChannelHoppingConfig_t Struct Reference
Wrapper struct that will contain the sequence of RAIL_BLE_TxChannelHoppingConfigEntry_t that represents the channel sequence to use during TX Channel Hopping.
#include <
rail_ble.h
>
Data Fields |
|
| uint32_t * | buffer |
|
Pointer to contiguous global read-write memory that will be used by RAIL to store channel hopping information throughout its operation.
|
|
| uint16_t | bufferLength |
|
This parameter must be set to the length of the buffer array.
|
|
| uint8_t | numberOfChannels |
|
The number of channels that is in the channel hopping sequence.
|
|
| uint8_t | reserved |
|
Pad bytes reserved for future use and currently ignored.
|
|
| RAIL_BLE_TxChannelHoppingConfigEntry_t * | entries |
|
A pointer to the first element of an array of
RAIL_BLE_TxChannelHoppingConfigEntry_t
that represents the channels used during channel hopping.
|
|
Wrapper struct that will contain the sequence of RAIL_BLE_TxChannelHoppingConfigEntry_t that represents the channel sequence to use during TX Channel Hopping.
Definition at line
888
of file
rail_ble.h
.
Field Documentation
◆ buffer
| uint32_t* RAIL_BLE_TxChannelHoppingConfig_t::buffer |
Pointer to contiguous global read-write memory that will be used by RAIL to store channel hopping information throughout its operation.
It need not be initialized and applications should never write data anywhere in this buffer.
Definition at line
895
of file
rail_ble.h
.
◆ bufferLength
| uint16_t RAIL_BLE_TxChannelHoppingConfig_t::bufferLength |
This parameter must be set to the length of the buffer array.
This way, during configuration, the software can confirm it's writing within the range of the buffer. The configuration API will return an error if bufferLength is insufficient.
Definition at line
902
of file
rail_ble.h
.
◆ entries
| RAIL_BLE_TxChannelHoppingConfigEntry_t * RAIL_BLE_TxChannelHoppingConfig_t::entries |
A pointer to the first element of an array of RAIL_BLE_TxChannelHoppingConfigEntry_t that represents the channels used during channel hopping.
The length of this array must be numberOfChannels.
Definition at line
915
of file
rail_ble.h
.
◆ numberOfChannels
| uint8_t RAIL_BLE_TxChannelHoppingConfig_t::numberOfChannels |
The number of channels that is in the channel hopping sequence.
Definition at line
904
of file
rail_ble.h
.
The documentation for this struct was generated from the following file:
-
protocol/ble/
rail_ble.h