RAIL_StateTiming_t Struct Reference
A timing configuration structure for the RAIL State Machine.
#include <
rail_types.h
>
Data Fields |
|
| RAIL_TransitionTime_t | idleToRx |
|
Transition time from IDLE to RX.
|
|
| RAIL_TransitionTime_t | txToRx |
|
Transition time from TX to RX.
|
|
| RAIL_TransitionTime_t | idleToTx |
|
Transition time from IDLE to RX.
|
|
| RAIL_TransitionTime_t | rxToTx |
|
Transition time from RX packet to TX.
|
|
| RAIL_TransitionTime_t | rxSearchTimeout |
|
Length of time the radio will search for a packet when coming from idle or RX.
|
|
| RAIL_TransitionTime_t | txToRxSearchTimeout |
|
Length of time the radio will search for a packet when coming from TX.
|
|
| RAIL_TransitionTime_t | txToTx |
|
Transition time from TX packet to TX.
|
|
A timing configuration structure for the RAIL State Machine.
Configure the timings of the radio state transitions for common situations. All of the listed timings are in microseconds. Transitions from an active radio state to idle are not configurable, and will always happen as fast as possible. No timing value can exceed RAIL_MAXIMUM_TRANSITION_US . Use RAIL_TRANSITION_TIME_KEEP to keep an existing setting.
For idleToRx, idleToTx, rxToTx, txToRx, and txToTx a value of 0 for the transition time means that the specified transition should happen as fast as possible, even if the timing cannot be as consistent. Otherwise, the timing value cannot be below RAIL_MINIMUM_TRANSITION_US .
For idleToTx, rxToTx, and txToTx setting a longer RAIL_TxPowerConfig_t::rampTime may result in a larger minimum value.
For rxSearchTimeout and txToRxSearchTimeout, there is no minimum value. A value of 0 disables the feature, functioning as an infinite timeout.
Definition at line
4472
of file
rail_types.h
.
Field Documentation
◆ idleToRx
| RAIL_TransitionTime_t RAIL_StateTiming_t::idleToRx |
Transition time from IDLE to RX.
Definition at line
4473
of file
rail_types.h
.
◆ idleToTx
| RAIL_TransitionTime_t RAIL_StateTiming_t::idleToTx |
Transition time from IDLE to RX.
Definition at line
4475
of file
rail_types.h
.
◆ rxSearchTimeout
| RAIL_TransitionTime_t RAIL_StateTiming_t::rxSearchTimeout |
Length of time the radio will search for a packet when coming from idle or RX.
Definition at line
4477
of file
rail_types.h
.
◆ rxToTx
| RAIL_TransitionTime_t RAIL_StateTiming_t::rxToTx |
Transition time from RX packet to TX.
Definition at line
4476
of file
rail_types.h
.
◆ txToRx
| RAIL_TransitionTime_t RAIL_StateTiming_t::txToRx |
Transition time from TX to RX.
Definition at line
4474
of file
rail_types.h
.
◆ txToRxSearchTimeout
| RAIL_TransitionTime_t RAIL_StateTiming_t::txToRxSearchTimeout |
Length of time the radio will search for a packet when coming from TX.
Definition at line
4479
of file
rail_types.h
.
◆ txToTx
| RAIL_TransitionTime_t RAIL_StateTiming_t::txToTx |
Transition time from TX packet to TX.
Definition at line
4481
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h