Energy Friendly Front End Module (EFF)
APIs for configuring and controlling an attached Energy Friendly Front End Module (EFF).
Data Structures |
|
| struct | RAIL_FemProtectionConfig_t |
|
Temperature protection configuration for the attached FEM.
|
|
| struct | RAIL_EffConfig_t |
|
Configuration data for the attached EFF device.
|
|
Macros |
|
| #define | RAIL_TEMP_MEASURE_COUNT (13U) |
|
Number of temperature values provided by
RAIL_GetTemperature()
.
|
|
| #define | RAIL_EFF_CONTROL_SIZE (52U) |
|
Number of bytes provided by
RAIL_GetSetEffControl()
.
|
|
| #define | RAIL_EFF_SUPPORTS_TRANSMIT (x) |
|
A macro that checks for EFFxx devices that support high power transmit.
|
|
| #define | RAIL_EFF_SUPPORTS_RECEIVE (x) |
|
A macro that checks for EFFxx devices that support receive.
|
|
Enumerations |
|
| enum |
RAIL_EffDevice_t
{
RAIL_EFF_DEVICE_NONE = 0, RAIL_EFF_DEVICE_EFF01Z11 , RAIL_EFF_DEVICE_EFF01A12 , RAIL_EFF_DEVICE_COUNT } |
|
EFF part numbers.
|
|
| enum |
RAIL_EffLnaMode_t
{
RAIL_EFF_LNA_MODE_RURAL = (0x01U << 0), RAIL_EFF_LNA_MODE_URBAN = (0x01U << 1), RAIL_EFF_LNA_MODE_BYPASS = (0x01U << 2), RAIL_EFF_LNA_MODE_COUNT = (0x01U << 3) } |
|
EFF LNA Modes.
|
|
| enum |
RAIL_ClpcEnable_t
{
RAIL_EFF_CLPC_DISABLED = 0, RAIL_EFF_CLPC_MODE_CHANGE = 1, RAIL_EFF_CLPC_POWER_SLOW = 2, RAIL_EFF_CLPC_POWER_FAST = 3, RAIL_EFF_CLPC_POWER_BOTH = 4, RAIL_EFF_CLPC_POWER_SLOW_BELOW_MAX = 5, RAIL_EFF_CLPC_POWER_FAST_BELOW_MAX = 6, RAIL_EFF_CLPC_POWER_BOTH_BELOW_MAX = 7, RAIL_EFF_CLPC_COUNT = 8 } |
|
EFF Closed Loop Power Control (CLPC) Enable states.
|
|
Functions |
|
| RAIL_Status_t | RAIL_ConfigEff ( RAIL_Handle_t railHandle, const RAIL_EffConfig_t *config) |
|
Configure the attached EFF device.
|
|
| RAIL_Status_t | RAIL_GetTemperature ( RAIL_Handle_t railHandle, int16_t tempBuffer[(13U)], bool reset) |
|
Get the different temperature measurements in Kelvin done by sequencer or host.
|
|
| RAIL_Status_t | RAIL_SetFemProtectionConfig ( RAIL_Handle_t railHandle, const RAIL_FemProtectionConfig_t *newFemConfig) |
|
Set the FEM maximum power for continuous TX and the duty cycle for TX operations from
RAIL_FemProtectionConfig_t
.
|
|
| RAIL_Status_t | RAIL_GetFemProtectionConfig ( RAIL_Handle_t railHandle, RAIL_FemProtectionConfig_t *femConfig) |
|
Get the FEM protection configuration.
|
|
| RAIL_Status_t | RAIL_GetSetEffControl ( RAIL_Handle_t railHandle, uint16_t tempBuffer[(52U)/sizeof(uint16_t)], bool reset) |
|
Get the different EFF Control measurements.
|
|
| RAIL_Status_t | RAIL_GetSetEffMode ( RAIL_Handle_t railHandle, uint8_t *newMode, bool changeMode) |
|
Copy the current FEM_DATA pin values into newMode.
|
|
| RAIL_Status_t | RAIL_GetSetEffRuralUrbanMv ( RAIL_Handle_t railHandle, uint16_t *newTrip, bool changeTrip) |
|
Copy the current Rural to Urban trip voltage into newTrip.
|
|
| RAIL_Status_t | RAIL_GetSetEffUrbanBypassMv ( RAIL_Handle_t railHandle, uint16_t *newTrip, bool changeTrip) |
|
Copy the current Urban to Bypass trip voltage into newTrip.
|
|
| RAIL_Status_t | RAIL_GetSetEffUrbanDwellTimeMs ( RAIL_Handle_t railHandle, uint32_t *newDwellTime, bool changeDwellTime) |
|
Copy the current Urban dwell time into newDwellTime.
|
|
| RAIL_Status_t | RAIL_GetSetEffBypassDwellTimeMs ( RAIL_Handle_t railHandle, uint32_t *newDwellTime, bool changeDwellTime) |
|
Copy the current Bypass dwell time into newDwellTime.
|
|
| RAIL_Status_t | RAIL_GetSetClpcSlowLoop ( RAIL_Handle_t railHandle, uint16_t *newTarget, uint16_t *newSlope, bool changeValues) |
|
Copy the current CLPC Slow Loop values into newTarget and newSlope.
|
|
| RAIL_Status_t | RAIL_GetSetClpcFastLoop ( RAIL_Handle_t railHandle, uint16_t *newTarget, uint16_t *newSlope, bool changeValues) |
|
Copy the current CLPC Fast Loop values into newTarget and newSlope.
|
|
| RAIL_Status_t | RAIL_GetSetClpcEnable ( RAIL_Handle_t railHandle, uint8_t *newClpcEnable, bool changeClpcEnable) |
|
Copy the current CLPC Enable in to newClpcEnable.
|
|
| RAIL_Status_t | RAIL_GetSetEffTempThreshold ( RAIL_Handle_t railHandle, uint16_t *newThreshold, bool changeThreshold) |
|
Get and set the EFF temperature threshold.
|
|
| RAIL_Status_t | RAIL_GetSetInternalTempThreshold ( RAIL_Handle_t railHandle, uint16_t *newThreshold, bool changeThreshold) |
|
Get and set the internal temperature threshold.
|
|
Detailed Description
APIs for configuring and controlling an attached Energy Friendly Front End Module (EFF).
The EFF is a high-performance, transmit/receive (T/R) front end module (FEM) for sub-GHz EFR32 devices. RAIL includes built-in functionality to transmit and receive via an attached EFF. This functionality optimizes RF performance while ensuring that the EFF stays within safe operating temperature limits.
Configuration and control of the EFF is performed by the Energy Friendly Front End Module (EFF) Utility .
- Note
- The EFF is only supported with EFR32XG25 devices.
Macro Definition Documentation
◆ RAIL_EFF_CONTROL_SIZE
| #define RAIL_EFF_CONTROL_SIZE (52U) |
Number of bytes provided by RAIL_GetSetEffControl() .
Definition at line
5664
of file
rail.h
.
◆ RAIL_EFF_SUPPORTS_RECEIVE
| #define RAIL_EFF_SUPPORTS_RECEIVE | ( |
x
|
) |
A macro that checks for EFFxx devices that support receive.
Definition at line
4294
of file
rail_types.h
.
◆ RAIL_EFF_SUPPORTS_TRANSMIT
| #define RAIL_EFF_SUPPORTS_TRANSMIT | ( |
x
|
) |
A macro that checks for EFFxx devices that support high power transmit.
Definition at line
4288
of file
rail_types.h
.
◆ RAIL_TEMP_MEASURE_COUNT
| #define RAIL_TEMP_MEASURE_COUNT (13U) |
Number of temperature values provided by RAIL_GetTemperature() .
Definition at line
5620
of file
rail.h
.
Enumeration Type Documentation
◆ RAIL_ClpcEnable_t
| enum RAIL_ClpcEnable_t |
EFF Closed Loop Power Control (CLPC) Enable states.
The EFF CLPC Enable state is passed to RAIL_ConfigEff() as the RAIL_EffConfig_t::clpcEnable . The Energy Friendly Front End Module (EFF) Utility uses advanced power controls to tune EFF output to match Surface Acoustic Wave (SAW) filter losses and antenna performance.
Definition at line
4323
of file
rail_types.h
.
◆ RAIL_EffDevice_t
| enum RAIL_EffDevice_t |
EFF part numbers.
The part number of the attached EFF device is passed to RAIL_ConfigEff() as RAIL_EffConfig_t::device . The Energy Friendly Front End Module (EFF) Utility configures and controls the EFF based on the capabilities of the attached EFF.
Definition at line
4278
of file
rail_types.h
.
◆ RAIL_EffLnaMode_t
| enum RAIL_EffLnaMode_t |
EFF LNA Modes.
The enabled EFF LNA modes are passed to RAIL_ConfigEff() as the RAIL_EffConfig_t::enabledLnaModes . The Energy Friendly Front End Module (EFF) Utility dynamically transitions between enabled LNA modes to maximize receive performance.
Definition at line
4307
of file
rail_types.h
.
Function Documentation
◆ RAIL_ConfigEff()
| RAIL_Status_t RAIL_ConfigEff | ( | RAIL_Handle_t |
railHandle,
|
| const RAIL_EffConfig_t * |
config
|
||
| ) |
Configure the attached EFF device.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] configA pointer to a RAIL_EffConfig_t struct that contains configuration data for the EFF.
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetFemProtectionConfig()
| RAIL_Status_t RAIL_GetFemProtectionConfig | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_FemProtectionConfig_t * |
femConfig
|
||
| ) |
Get the FEM protection configuration.
- Parameters
-
[in] railHandleA RAIL instance handle. [out] femConfigCurrent FEM protection configuration written to this pointer.
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetSetClpcEnable()
| RAIL_Status_t RAIL_GetSetClpcEnable | ( | RAIL_Handle_t |
railHandle,
|
| uint8_t * |
newClpcEnable,
|
||
| bool |
changeClpcEnable
|
||
| ) |
Copy the current CLPC Enable in to newClpcEnable.
If changeClpcEnable is true, update current CLPC Enable with newClpcEnable first.
- Parameters
-
[in] railHandleA RAIL instance handle [in,out] newClpcEnableA pointer to a uint8_t that will contain the CLPC Enable [in] changeClpcEnableIf true, use newClpcEnable to update the current CLPC Enable
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetSetClpcFastLoop()
| RAIL_Status_t RAIL_GetSetClpcFastLoop | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t * |
newTarget,
|
||
| uint16_t * |
newSlope,
|
||
| bool |
changeValues
|
||
| ) |
Copy the current CLPC Fast Loop values into newTarget and newSlope.
If changeTarget is true, update current CLPC Fast Loop Target and Slope first.
- Parameters
-
[in] railHandleA RAIL instance handle [in,out] newTargetA pointer to a uint16_t that will contain the CLPC Fast Loop Target [in,out] newSlopeA pointer to a uint16_t that will contain the CLPC Fast Loop Slope [in] changeValuesIf true, use newTarget and newGain to update the CLPC Fast Loop values
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetSetClpcSlowLoop()
| RAIL_Status_t RAIL_GetSetClpcSlowLoop | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t * |
newTarget,
|
||
| uint16_t * |
newSlope,
|
||
| bool |
changeValues
|
||
| ) |
Copy the current CLPC Slow Loop values into newTarget and newSlope.
If changeTarget is true, update current CLPC Slow Loop Target and Slope first.
- Parameters
-
[in] railHandleA RAIL instance handle [in,out] newTargetA pointer to a uint16_t that will contain the CLPC Slow Loop Target [in,out] newSlopeA pointer to a uint16_t that will contain the CLPC Slow Loop Slope [in] changeValuesIf true, use newTarget and newGain to update the CLPC SLow Loop values
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetSetEffBypassDwellTimeMs()
| RAIL_Status_t RAIL_GetSetEffBypassDwellTimeMs | ( | RAIL_Handle_t |
railHandle,
|
| uint32_t * |
newDwellTime,
|
||
| bool |
changeDwellTime
|
||
| ) |
Copy the current Bypass dwell time into newDwellTime.
If changeDwellTime is true, update current Bypass dwell time with newDwellTime first.
- Parameters
-
[in] railHandleA RAIL instance handle [in,out] newDwellTimeA pointer to a uint16_t that will contain the Bypass dwell dwell time, in milliseconds [in] changeDwellTimeIf true, use newDwellTime to update current Bypass dwell time
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetSetEffControl()
| RAIL_Status_t RAIL_GetSetEffControl | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
tempBuffer[(52U)/sizeof(uint16_t)],
|
||
| bool |
reset
|
||
| ) |
Get the different EFF Control measurements.
- Parameters
-
[in] railHandleA RAIL instance handle. [out] tempBufferThe address of the target array. tempBuffer array must be at least RAIL_EFF_CONTROL_SIZE bytes. [in] resetReset the EFF Control measurements.
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetSetEffMode()
| RAIL_Status_t RAIL_GetSetEffMode | ( | RAIL_Handle_t |
railHandle,
|
| uint8_t * |
newMode,
|
||
| bool |
changeMode
|
||
| ) |
Copy the current FEM_DATA pin values into newMode.
If changeMode is true, update FEM_DATA pin values with newMode first.
- Parameters
-
[in] railHandleA RAIL instance handle [in,out] newModeA pointer to a uint8_t that will contain the FEM_DATA pin values [in] changeModeIf true, use newMode to update FEM_DATA pin values
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetSetEffRuralUrbanMv()
| RAIL_Status_t RAIL_GetSetEffRuralUrbanMv | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t * |
newTrip,
|
||
| bool |
changeTrip
|
||
| ) |
Copy the current Rural to Urban trip voltage into newTrip.
If changeTrip is true, update current Rural to Urban trip voltage with newTrip first.
- Parameters
-
[in] railHandleA RAIL instance handle [in,out] newTripA pointer to a uint16_t that will contain the Rural to Urban trip voltage, in millivolts [in] changeTripIf true, use newTrip to update current Rural to Urban trip voltage
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetSetEffTempThreshold()
| RAIL_Status_t RAIL_GetSetEffTempThreshold | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t * |
newThreshold,
|
||
| bool |
changeThreshold
|
||
| ) |
Get and set the EFF temperature threshold.
The EFR32 device periodically takes temperature measurements of the attached EFF device. If the EFF temperature ever exceeds the EFF temperature threshold, any active transmit operation is aborted and future transmit operations are blocked until the EFF temperature falls below the threshold.
- Parameters
-
[in] railHandleA RAIL instance handle [in,out] newThresholdA pointer to a uint16_t that will contain the EFF temperature threshold, in Kelvin [in] changeThresholdIf true, use changeThreshold to update current EFF temperature threshold
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetSetEffUrbanBypassMv()
| RAIL_Status_t RAIL_GetSetEffUrbanBypassMv | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t * |
newTrip,
|
||
| bool |
changeTrip
|
||
| ) |
Copy the current Urban to Bypass trip voltage into newTrip.
If changeTrip is true, update current Urban to Bypass trip voltage with newTrip first.
- Parameters
-
[in] railHandleA RAIL instance handle [in,out] newTripA pointer to a uint16_t that will contain the Urban to Bypass trip voltage, in millivolts [in] changeTripIf true, use newTrip to update current Urban to Bypass trip voltage
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetSetEffUrbanDwellTimeMs()
| RAIL_Status_t RAIL_GetSetEffUrbanDwellTimeMs | ( | RAIL_Handle_t |
railHandle,
|
| uint32_t * |
newDwellTime,
|
||
| bool |
changeDwellTime
|
||
| ) |
Copy the current Urban dwell time into newDwellTime.
If changeDwellTime is true, update current Urban dwell time with newDwellTime first.
- Parameters
-
[in] railHandleA RAIL instance handle [in,out] newDwellTimeA pointer to a uint16_t that will contain the Urban dwell dwell time, in milliseconds [in] changeDwellTimeIf true, use newDwellTime to update current Urban dwell time
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetSetInternalTempThreshold()
| RAIL_Status_t RAIL_GetSetInternalTempThreshold | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t * |
newThreshold,
|
||
| bool |
changeThreshold
|
||
| ) |
Get and set the internal temperature threshold.
The EFR32 device periodically takes measurements of its internal temperature when attached to an EFF device. If the internal temperature ever exceeds the internal temperature threshold, any active transmit operation is aborted and future transmit operations are blocked until the internal temperature falls below the threshold.
- Parameters
-
[in] railHandleA RAIL instance handle [in,out] newThresholdA pointer to a uint16_t that will contain the internal temperature threshold, in Kelvin [in] changeThresholdIf true, use changeThreshold to update current internal temperature threshold
- Returns
- Status code indicating success of the function call.
◆ RAIL_GetTemperature()
| RAIL_Status_t RAIL_GetTemperature | ( | RAIL_Handle_t |
railHandle,
|
| int16_t |
tempBuffer[(13U)],
|
||
| bool |
reset
|
||
| ) |
Get the different temperature measurements in Kelvin done by sequencer or host.
Values that are not populated yet or incorrect are set to 0.
- Parameters
-
[in] railHandleA RAIL instance handle. [out] tempBufferThe address of the array that will contain temperatures. tempBuffer array must be at least RAIL_TEMP_MEASURE_COUNT int16_t. [in] resetReset the EFF temperature values.
- Returns
- Status code indicating success of the function call.
◆ RAIL_SetFemProtectionConfig()
| RAIL_Status_t RAIL_SetFemProtectionConfig | ( | RAIL_Handle_t |
railHandle,
|
| const RAIL_FemProtectionConfig_t * |
newFemConfig
|
||
| ) |
Set the FEM maximum power for continuous TX and the duty cycle for TX operations from RAIL_FemProtectionConfig_t .
Default continuous TX power is defined at 200 deci-dBm and can be set to a maximum of 300 deci-dBm. Default duty cycle is defined at 50 percent and can be set to a maximum of 100 percent.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] newFemConfigPointer to the new limits to use for the FEM protection configuration
- Returns
- Status code indicating success of the function call.
- Note
- Setting the power for continuous TX and the duty cycle from RAIL_FemProtectionConfig_t to 0 will apply their default value. For an ambient temperature above 70 degrees Celsius, it is recommended to use the default configuration.