RAIL_ZWAVE_BeamRxConfig_t Struct Reference

Configuration structure for Z-Wave Beam Detection.

#include < rail_zwave.h >

Data Fields

RAIL_RxChannelHoppingConfig_t channelHoppingConfig
Channel hopping pattern to use for beam detection.
RAIL_RxDutyCycleConfig_t receiveConfig_100
Amount of time to spend trying to receive a beam once detected.
RAIL_RxDutyCycleConfig_t receiveConfig_40
Amount of time to spend trying to receive a beam once detected.

Configuration structure for Z-Wave Beam Detection.

This structure should not be used without direct instruction by Silicon Labs. Appropriate defaults for this are built into the RAIL library.

Definition at line 365 of file rail_zwave.h .

Field Documentation

receiveConfig_100

RAIL_RxDutyCycleConfig_t RAIL_ZWAVE_BeamRxConfig_t::receiveConfig_100

Amount of time to spend trying to receive a beam once detected.

100kbps only

Definition at line 370 of file rail_zwave.h .

receiveConfig_40

RAIL_RxDutyCycleConfig_t RAIL_ZWAVE_BeamRxConfig_t::receiveConfig_40

Amount of time to spend trying to receive a beam once detected.

40kbps only

Definition at line 373 of file rail_zwave.h .


The documentation for this struct was generated from the following file:
  • protocol/zwave/ rail_zwave.h