RAIL_ZWAVE_LrAckData_t Struct Reference

Configuration structure for Z-Wave Long Range ACK.

#include < rail_zwave.h >

Data Fields

int8_t noiseFloorDbm
Radio noise level measured on the channel the frame is transmitted on.
int8_t txPowerDbm
Transmit power used to transmit the ongoing Z-Wave Long Range ACK.
int8_t receiveRssiDbm
Signal strength measured while receiving the Z-Wave Long Range frame.

Configuration structure for Z-Wave Long Range ACK.

Definition at line 349 of file rail_zwave.h .


The documentation for this struct was generated from the following file:
  • protocol/zwave/ rail_zwave.h