RAIL_ZWAVE_RegionConfig_t Struct Reference

Each Z-Wave region supports 3 channels.

#include < rail_zwave.h >

Data Fields

uint32_t frequency [(4U)]
Channel frequency in hertz.
RAIL_TxPower_t maxPower [(4U)]
The maximum power allowed on the channel.
RAIL_ZWAVE_Baud_t baudRate [(4U)]
Channel baud rate index.
RAIL_ZWAVE_RegionId_t regionId
Identification number for the region.

Each Z-Wave region supports 3 channels.

Definition at line 385 of file rail_zwave.h .


The documentation for this struct was generated from the following file:
  • protocol/zwave/ rail_zwave.h