RAIL_BLE_AoxConfig_t Struct Reference
Contains arguments for RAIL_BLE_ConfigAox function.
#include <
rail_ble.h
>
Data Fields |
|
| RAIL_BLE_AoxOptions_t | aoxOptions |
|
See RAIL_BLE_AOX_OPTIONS_* for bitfield defines for different AoX features.
|
|
| uint16_t | cteBuffSize |
|
Size of the raw AoX CTE (continuous tone extension) data capture buffer in bytes.
|
|
| uint32_t * | cteBuffAddr |
|
Address to where the received CTE is written.
|
|
| uint8_t * | antArrayAddr |
|
Address to first element of antenna pattern array.
|
|
| uint8_t | antArraySize |
|
Size of the antenna pattern array.
|
|
Contains arguments for RAIL_BLE_ConfigAox function.
Definition at line
639
of file
rail_ble.h
.
Field Documentation
◆ antArrayAddr
| uint8_t* RAIL_BLE_AoxConfig_t::antArrayAddr |
Address to first element of antenna pattern array.
Array must be in RAM. Each element of the array contains an antenna number. The switching pattern is defined by the order of antennas in this array.
Definition at line
658
of file
rail_ble.h
.
The documentation for this struct was generated from the following file:
-
protocol/ble/
rail_ble.h