Received packet details obtained via RAIL_GetRxPacketDetails() or RAIL_GetRxPacketDetailsAlt() .
#include <
rail_types.h
>
Data Fields |
|
| RAIL_PacketTimeStamp_t | timeReceived |
|
The timestamp of the received packet in the RAIL timebase.
|
|
| bool | crcPassed |
|
Indicates whether the CRC passed or failed for the received packet.
|
|
| bool | isAck |
|
Indicate whether the received packet was the expected ACK.
|
|
| int8_t | rssi |
|
RSSI of the received packet in integer dBm.
|
|
| uint8_t | lqi |
|
The link quality indicator of the received packet.
|
|
| uint8_t | syncWordId |
|
For radios and PHY configurations that support multiple sync words, this number is the ID of the sync word that was used for this packet.
|
|
| uint8_t | subPhyId |
|
In configurations where the radio has the option of receiving a given packet in multiple ways, indicates which of the sub-PHY options was used to receive the packet.
|
|
| uint8_t | antennaId |
|
For
Antenna Control
configurations where the device has multiple antennas, this indicates which antenna received the packet.
|
|
| uint8_t | channelHoppingChannelIndex |
|
When channel hopping is enabled, this field will contain the index of the channel in
RAIL_RxChannelHoppingConfig_t::entries
on which this packet was received, or a sentinel value.
|
|
| uint16_t | channel |
|
The channel on which the packet was received.
|
|
Received packet details obtained via RAIL_GetRxPacketDetails() or RAIL_GetRxPacketDetailsAlt() .
- Note
- Certain details are always available, while others are only available if the RAIL_RxOptions_t RAIL_RX_OPTION_REMOVE_APPENDED_INFO option is not in effect and the received packet's RAIL_RxPacketStatus_t is among the RAIL_RX_PACKET_READY_ set. Each detail's description indicates its availability.
Definition at line
3325
of file
rail_types.h
.
Field Documentation
◆ antennaId
| uint8_t RAIL_RxPacketDetails_t::antennaId |
For Antenna Control configurations where the device has multiple antennas, this indicates which antenna received the packet.
When there is only one antenna, this will be set to the default of 0.
It is always available.
Definition at line
3416
of file
rail_types.h
.
◆ channel
| uint16_t RAIL_RxPacketDetails_t::channel |
The channel on which the packet was received.
It is always available.
- Note
- It is best to fully process (empty or clear) the receive FIFO before changing channel configurations ( RAIL_ConfigChannels() or a built-in configuration) as unprocessed packets' channel could reflect the wrong configuration. On EFR32xG1 only this advice also applies when changing channels for receive or transmit where unprocessed packets' channel could reflect the new channel.
Definition at line
3439
of file
rail_types.h
.
◆ channelHoppingChannelIndex
| uint8_t RAIL_RxPacketDetails_t::channelHoppingChannelIndex |
When channel hopping is enabled, this field will contain the index of the channel in RAIL_RxChannelHoppingConfig_t::entries on which this packet was received, or a sentinel value.
On EFR32XG1 parts, on which channel hopping is not supported, this value is still part of the structure, but will be a meaningless value.
It is always available.
Definition at line
3426
of file
rail_types.h
.
◆ crcPassed
| bool RAIL_RxPacketDetails_t::crcPassed |
Indicates whether the CRC passed or failed for the received packet.
It is true for RAIL_RX_PACKET_READY_SUCCESS packets and false for all others.
It is always available.
Definition at line
3339
of file
rail_types.h
.
◆ isAck
| bool RAIL_RxPacketDetails_t::isAck |
Indicate whether the received packet was the expected ACK.
It is true for the expected ACK and false otherwise.
It is always available.
An expected ACK is defined as a protocol-correct ACK packet successfully-received ( RAIL_RX_PACKET_READY_SUCCESS or RAIL_RX_PACKET_READY_CRC_ERROR ) and whose sync word was detected within the RAIL_AutoAckConfig_t::ackTimeout period following a transmit which specified RAIL_TX_OPTION_WAIT_FOR_ACK , requested an ACK, and auto-ACK is enabled. When true, the ackTimeout period was terminated so no RAIL_EVENT_RX_ACK_TIMEOUT will be subsequently posted for the transmit.
A "protocol-correct ACK" applies to the 802.15.4 or Z-Wave protocols for which RAIL can discern the frame type and match the ACK's sequence number with that of the transmitted frame. For other protocols, the first packet successfully-received whose sync word was detected within the ackTimeout period is considered the expected ACK; upper layers are responsible for confirming this.
Definition at line
3364
of file
rail_types.h
.
◆ lqi
| uint8_t RAIL_RxPacketDetails_t::lqi |
The link quality indicator of the received packet.
A zero would indicate a very low quality packet while a 255 would indicate a very high quality packet.
When not available it will be 0.
Definition at line
3379
of file
rail_types.h
.
◆ rssi
| int8_t RAIL_RxPacketDetails_t::rssi |
RSSI of the received packet in integer dBm.
It is latched when the sync word is detected for the packet.
When not available it will be RAIL_RSSI_INVALID_DBM .
Definition at line
3371
of file
rail_types.h
.
◆ subPhyId
| uint8_t RAIL_RxPacketDetails_t::subPhyId |
In configurations where the radio has the option of receiving a given packet in multiple ways, indicates which of the sub-PHY options was used to receive the packet.
Most radio configurations do not have this ability and the subPhyId is set to 0.
Currently, this field is used by the BLE Coded PHY, the BLE Simulscan PHY and the SUN OFDM PHYs. In BLE cases, a value of 0 marks a 500 kbps packet, a value of 1 marks a 125 kbps packet, and a value of 2 marks a 1 Mbps packet. Also, see RAIL_BLE_ConfigPhyCoded and RAIL_BLE_ConfigPhySimulscan .
In SUN OFDM cases, the value corresponds to the numerical value of the Modulation and Coding Scheme (MCS) level of the last received packet. The packet bitrate depends on the MCS value, as well as the OFDM option. Packets bitrates for SUN OFDM PHYs can be found in 802.15.4-2020 specification, chapter 20.3, table 20-10. Ex: Packet bitrate for OFDM option 1 MCS0 is 100kb/s and 2400kb/s for MCS6.
It is always available.
Definition at line
3408
of file
rail_types.h
.
◆ syncWordId
| uint8_t RAIL_RxPacketDetails_t::syncWordId |
For radios and PHY configurations that support multiple sync words, this number is the ID of the sync word that was used for this packet.
It is always available.
Definition at line
3386
of file
rail_types.h
.
◆ timeReceived
| RAIL_PacketTimeStamp_t RAIL_RxPacketDetails_t::timeReceived |
The timestamp of the received packet in the RAIL timebase.
When not available it will be RAIL_PACKET_TIME_INVALID .
Definition at line
3331
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h