USB DEVICE protocol stack, see USB Device Stack Library page for detailed documentation.
.
Data Structures | |
struct | USBD_Init_TypeDef |
USB Device stack initialization structure. | |
struct | USBD_Callbacks_TypeDef |
USB Device stack callback structure. |
Typedefs | |
typedef void(* | USBD_UsbResetCb_TypeDef) (void) |
USB Reset callback function. | |
typedef void(* | USBD_SofIntCb_TypeDef) (uint16_t sofNr) |
USB Start Of Frame (SOF) interrupt callback function. | |
typedef void(* | USBD_DeviceStateChangeCb_TypeDef) (USBD_State_TypeDef oldState, USBD_State_TypeDef newState) |
USB State change callback function. | |
typedef bool(* | USBD_IsSelfPoweredCb_TypeDef) (void) |
USB power mode callback function. | |
typedef int(* | USBD_SetupCmdCb_TypeDef) (const USB_Setup_TypeDef *setup) |
USB setup request callback function. | |
typedef struct USBD_Callbacks_TypeDef | USBD_Callbacks_TypeDef |
USB Device stack callback structure. |
Enumerations | |
enum | USBD_State_TypeDef { USBD_STATE_NONE = 0, USBD_STATE_ATTACHED = 1, USBD_STATE_POWERED = 2, USBD_STATE_DEFAULT = 3, USBD_STATE_ADDRESSED = 4, USBD_STATE_CONFIGURED = 4, USBD_STATE_SUSPENDED = 6, USBD_STATE_LASTMARKER = 7 } |
USB device state enumerator. |
Functions | |
void | USBD_AbortAllTransfers (void) |
Abort all pending transfers. | |
int | USBD_AbortTransfer (int epAddr) |
Abort a pending transfer on a specific endpoint. | |
void | USBD_Connect (void) |
Start USB device operation. | |
void | USBD_Disconnect (void) |
Stop USB device operation. | |
bool | USBD_EpIsBusy (int epAddr) |
Check if an endpoint is busy doing a transfer. | |
USBD_State_TypeDef | USBD_GetUsbState (void) |
Get current USB device state. | |
const char * | USBD_GetUsbStateName (USBD_State_TypeDef state) |
Get a string naming a device USB state. | |
int | USBD_Init (const USBD_Init_TypeDef *p) |
Initializes USB device hardware and internal protocol stack data structures, then connects the data-line (D+ or D-) pullup resistor to signal host that enumeration can begin. | |
int | USBD_Read (int epAddr, void *data, int byteCount, USB_XferCompleteCb_TypeDef callback) |
Start a read (OUT) transfer on an endpoint. | |
int | USBD_RemoteWakeup (void) |
Perform a remote wakeup signalling sequence. | |
bool | USBD_SafeToEnterEM2 (void) |
int | USBD_StallEp (int epAddr) |
Set an endpoint in the stalled (halted) state. | |
void | USBD_Stop (void) |
Stop USB device stack operation. | |
int | USBD_UnStallEp (int epAddr) |
Reset stall state on a stalled (halted) endpoint. | |
int | USBD_Write (int epAddr, void *data, int byteCount, USB_XferCompleteCb_TypeDef callback) |
Start a write (IN) transfer on an endpoint. | |
void | usbSuspendDsr (void) |
USB suspend delayed service routine. |
Detailed Description
See em_usbd.c
for source code.
Typedef Documentation
typedef struct USBD_Callbacks_TypeDef USBD_Callbacks_TypeDef |
Callback functions used by the device stack to signal events or query status to/from the application. See USBD_Init_TypeDef. Assign members to NULL if your application don't need a specific callback.
typedef void(* USBD_DeviceStateChangeCb_TypeDef) (USBD_State_TypeDef oldState, USBD_State_TypeDef newState) |
Called whenever the device change state.
- Parameters
-
[in] oldState
The device USB state just leaved. See USBD_State_TypeDef. [in] newState
New (the current) USB device state. See USBD_State_TypeDef.
typedef bool(* USBD_IsSelfPoweredCb_TypeDef) (void) |
Called whenever the device stack needs to query if the device is currently self- or bus-powered. Typically when host has issued an GET_STATUS setup command.
- Returns
- True if self-powered, false otherwise.
typedef int(* USBD_SetupCmdCb_TypeDef) (const USB_Setup_TypeDef *setup) |
Called on each setup request received from host. This gives the application a possibility to extend or override standard requests, and to implement class or vendor specific requests. Return USB_STATUS_OK if the request is handled, return USB_STATUS_REQ_ERR if it is an illegal request or return USB_STATUS_REQ_UNHANDLED to pass the request on to the default request handler.
- Parameters
-
[in] setup
Pointer to an USB setup packet. See USB_Setup_TypeDef.
- Returns
- An appropriate status/error code. See USB_Status_TypeDef.
typedef void(* USBD_SofIntCb_TypeDef) (uint16_t sofNr) |
Called at each SOF interrupt (if enabled),
- Parameters
-
[in] sofNr
Current frame number. The value rolls over to 0 after 16383 (0x3FFF).
typedef void(* USBD_UsbResetCb_TypeDef) (void) |
Called whenever USB reset signalling is detected on the USB port.
Enumeration Type Documentation
enum USBD_State_TypeDef |
Function Documentation
void USBD_AbortAllTransfers | ( | void |
| ) |
Aborts transfers for all endpoints currently in use. Pending transfers on the default endpoint (EP0) are not aborted.
References USB_STATUS_EP_ABORTED.
int USBD_AbortTransfer | ( | int | epAddr | ) |
- Parameters
-
[in] epAddr
The address of the endpoint to abort.
References assert, NULL, USB_STATUS_EP_ABORTED, USB_STATUS_OK, USBD_STATE_ADDRESSED, and USBD_STATE_CONFIGURED.
void USBD_Connect | ( | void |
| ) |
Device operation is started by connecting a pullup resistor on the appropriate USB data line.
void USBD_Disconnect | ( | void |
| ) |
Device operation is stopped by disconnecting the pullup resistor from the appropriate USB data line. Often referred to as a "soft" disconnect.
References USBD_STATE_SUSPENDED.
Referenced by USBD_Stop().
bool USBD_EpIsBusy | ( | int | epAddr | ) |
- Parameters
-
[in] epAddr
The address of the endpoint to check.
- Returns
- True if endpoint is busy, false otherwise.
Referenced by USBD_RemoteWakeup().
USBD_State_TypeDef USBD_GetUsbState | ( | void |
| ) |
- Returns
- Device USB state. See USBD_State_TypeDef.
Referenced by USBD_Read(), and USBD_Write().
const char * USBD_GetUsbStateName | ( | USBD_State_TypeDef | state | ) |
- Parameters
-
[in] state
Device USB state. See USBD_State_TypeDef.
- Returns
- State name string pointer.
References USBD_STATE_LASTMARKER.
int USBD_Init | ( | const USBD_Init_TypeDef * | p | ) |
- Note
- You may later use USBD_Disconnect() and USBD_Connect() to force reenumeration.
- Parameters
-
[in] p
Pointer to device initialization struct. See USBD_Init_TypeDef.
- Returns
- USB_STATUS_OK on success, else an appropriate error code.
References assert, USB_EndpointDescriptor_TypeDef::bEndpointAddress, USB_EndpointDescriptor_TypeDef::bmAttributes, USBD_Init_TypeDef::bufferingMultiplier, USBD_Init_TypeDef::callbacks, CONFIG_DESC_BM_TRANSFERTYPE, USBD_Init_TypeDef::configDescriptor, USBD_Init_TypeDef::deviceDescriptor, MEMSET, NULL, USBD_Init_TypeDef::numberOfStrings, USBD_Init_TypeDef::stringDescriptors, USB_ENDPOINT_DESCRIPTOR, USB_EP0_SIZE, USB_EPNUM_MASK, USB_EPTYPE_CTRL, USB_REMOTEWKUPEN_STATE, USB_SETUP_DIR_MASK, USB_STATUS_ILLEGAL, USB_STATUS_OK, USBD_STATE_LASTMARKER, USBD_STATE_NONE, USBTIMER_Init(), and USB_EndpointDescriptor_TypeDef::wMaxPacketSize.
int USBD_Read | ( | int | epAddr, |
void * | data, |
||
int | byteCount, |
||
USB_XferCompleteCb_TypeDef | callback |
||
) |
- Note
- The transfer buffer length must be a multiple of 4 bytes in length and WORD (4 byte) aligned. When allocating the buffer, round buffer length up. If it is possible that the host will send more data than your device expects, round buffer size up to the next multiple of maxpacket size.
- Parameters
-
[in] epAddr
Endpoint address. [in] data
Pointer to transfer data buffer. [in] byteCount
Transfer length. [in] callback
Function to be called on transfer completion. Supply NULL if no callback is needed. See USB_XferCompleteCb_TypeDef.
- Returns
- USB_STATUS_OK on success, else an appropriate error code.
References assert, NULL, USB_STATUS_DEVICE_UNCONFIGURED, USB_STATUS_EP_BUSY, USB_STATUS_EP_STALLED, USB_STATUS_OK, USBD_GetUsbState(), and USBD_STATE_CONFIGURED.
int USBD_RemoteWakeup | ( | void |
| ) |
- Note
- It is the responsibility of the application to ensure that remote wakeup is not attempted before the device has been suspended for at least 5 miliseconds. This function should not be called from within an interrupt handler.
- Returns
- USB_STATUS_OK on success, else an appropriate error code.
References elapsedTimeInt16u, FIFO_DEQUEUE, halCommonGetInt16uMillisecondTick(), MEMSET, NULL, USB_STATUS_ILLEGAL, USB_STATUS_OK, USB_STATUS_TIMEOUT, USBD_EpIsBusy(), USBD_STATE_SUSPENDED, USBD_Write(), usbForceTxData()
, and usbTxData()
.
bool USBD_SafeToEnterEM2 | ( | void |
| ) |
int USBD_StallEp | ( | int | epAddr | ) |
- Parameters
-
[in] epAddr
The address of the endpoint to stall.
- Returns
- USB_STATUS_OK on success, else an appropriate error code.
References assert, NULL, USB_STATUS_ILLEGAL, and USB_STATUS_OK.
void USBD_Stop | ( | void |
| ) |
The data-line pullup resistor is turned off, USB interrupts are disabled, and finally the USB pins are disabled.
References USBD_Disconnect(), and USBD_STATE_NONE.
int USBD_UnStallEp | ( | int | epAddr | ) |
- Parameters
-
[in] epAddr
The address of the endpoint to un-stall.
- Returns
- USB_STATUS_OK on success, else an appropriate error code.
References assert, NULL, USB_STATUS_ILLEGAL, and USB_STATUS_OK.
int USBD_Write | ( | int | epAddr, |
void * | data, |
||
int | byteCount, |
||
USB_XferCompleteCb_TypeDef | callback |
||
) |
- Parameters
-
[in] epAddr
Endpoint address. [in] data
Pointer to transfer data buffer. This buffer must be WORD (4 byte) aligned. [in] byteCount
Transfer length. [in] callback
Function to be called on transfer completion. Supply NULL if no callback is needed. See USB_XferCompleteCb_TypeDef.
- Returns
- USB_STATUS_OK on success, else an appropriate error code.
References assert, NULL, USB_STATUS_DEVICE_UNCONFIGURED, USB_STATUS_EP_BUSY, USB_STATUS_EP_STALLED, USB_STATUS_ILLEGAL, USB_STATUS_OK, USBD_GetUsbState(), and USBD_STATE_CONFIGURED.
Referenced by USBD_RemoteWakeup().
void usbSuspendDsr | ( | void |
| ) |
This function keeps the device in a low power state in order to meet USB specification during USB suspend state.
References emberStackPowerDown(), halSleep(), SLEEPMODE_IDLE, and USBD_STATE_SUSPENDED.