OTA Bootload Client Callbacks
Detailed Description
These callbacks are contributed by the OTA Bootload Client plugin.
Function Documentation
EmberZclStatus_t emberZclOtaBootloadClientDownloadCompleteCallback | ( | const EmberZclOtaBootloadFileSpec_t * | fileSpec, |
EmberZclStatus_t | status |
||
) |
An OTA file has been downloaded and verified, or failed to do one of the two.
- Parameters
-
fileSpec
The specification for the OTA file in question. status
The status of file download and verification.
- Returns
- A status based on the application's analysis of the downloaded file. This is an opportunity for the application to verify the downloaded image and return a related status.
- See also
- emberZclOtaBootloadStorageFind
bool emberZclOtaBootloadClientExpectSecureOta | ( |
| ) |
Determine expected server connection security
- Returns
true
if the specification requires a DTLS connection to the server
bool emberZclOtaBootloadClientGetQueryNextImageParametersCallback | ( | EmberZclOtaBootloadFileSpec_t * | fileSpec, |
EmberZclOtaBootloadHardwareVersion_t * | hardwareVersion |
||
) |
Get the parameters for a QueryNextImage command.
- Parameters
-
fileSpec
The OTA file specification to include in the query. hardwareVersion
The current hardware version of the device, or EMBER_ZCL_OTA_BOOTLOAD_HARDWARE_VERSION_NULL if this information is to be ignored.
- Returns
true
if the device should continue to send a QueryNextImage command, orfalse
if it should reschedule the command for a later time.
void emberZclOtaBootloadClientPreBootloadCallback | ( | const EmberZclOtaBootloadFileSpec_t * | fileSpec | ) |
An OTA file is about to be installed.
- Parameters
-
fileSpec
The specification for the OTA file that will be installed.
- See also
- emberZclOtaBootloadStorageFind
bool emberZclOtaBootloadClientServerDiscoveredCallback | ( | const EmberZclOtaBootloadClientServerInfo_t * | serverInfo | ) |
A potential OTA Server has been discovered.
- Parameters
-
serverInfo
Information about the discovered OTA Server device.
- Returns
true
if the device should be chosen as the OTA Server,false
otherwise.
- Note
- If
true
is returned, the OTA Client state machine will move to the next state, which is querying the OTA Server device for a new OTA file to download. Iffalse
is returned, the OTA Client will continue to try to discover an OTA Server.
bool emberZclOtaBootloadClientServerHasDiscByClusterId | ( | const EmberZclClusterSpec_t * | clusterSpec, |
EmberCoapResponseHandler | responseHandler |
||
) |
Initiate a server discovery
- Parameters
-
clusterSpec
server specifications responseHandler
function to handle the response to the CoAP message
- Returns
true
if the specification is valid and the request has been sent
- Note
- If
true
is returned, the OTA Client state machine will wait until the responseHandler is called
References emberZclDiscByClusterId().
bool emberZclOtaBootloadClientServerHasDnsNameCallback | ( | EmberZclOtaBootloadClientServerInfo_t * | serverInfo | ) |
Start a DNS hostname resolution
- Parameters
-
serverInfo
Updated to the default server parameters
- Returns
true
if the device should use the DNS hostname for the OTA Server
- Note
- If
true
is returned, the OTA Client state machine will wait for the DNS hostname to be resolved.
bool emberZclOtaBootloadClientServerHasStaticAddressCallback | ( | EmberZclOtaBootloadClientServerInfo_t * | serverInfo | ) |
Check to see if a static IP address should be used for the OTA server
- Parameters
-
serverInfo
Structure to store the OTA server parameters
- Returns
true
if the device should use a static address for the OTA Server
- Note
- If
true
is returned, the OTA Client state machine will move to the next state, which is querying the OTA Server device for a new OTA file to download. Iffalse
is returned, the OTA Client will continue to try to discover an OTA Server.
bool emberZclOtaBootloadClientSetVersionInfoCallback | ( |
| ) |
This function attempts to set the cluster attribute values to those in the policy parameters. The attributes affected are 'OTA Current File Version', 'Manufacturer ID', and 'Image Type ID'.
- Returns
true
if there was an error setting one of the attributes
bool emberZclOtaBootloadClientStartDownloadCallback | ( | const EmberZclOtaBootloadFileSpec_t * | fileSpec, |
bool | existingFile |
||
) |
A download of an OTA file can be started.
- Parameters
-
fileSpec
The specification for the OTA file to potentially be downloaded. existingFile
A file with this same specification currently exists in OTA storage.
- Returns
true
if the device should kick off the download process for this file, orfalse
if it should continue to query for new images.
- See also
- emberZclOtaBootloadStorageFind