EmberZclBindingEntry_t Struct Reference
#include <
zcl-core-types.h
>
Data Fields | |
EmberZclEndpointId_t | endpointId |
EmberZclClusterSpec_t | clusterSpec |
struct { | |
struct { | |
EmberZclScheme_t scheme | |
union { | |
EmberIpv6Address address | |
EmberZclUid_t uid | |
} data | |
EmberZclNetworkDestinationType_t type | |
uint16_t port | |
} network | |
EmberZclApplicationDestination_t application | |
} | destination |
EmberZclReportingConfigurationId_t | reportingConfigurationId |
This structure holds a binding entry.
Field Documentation
EmberIpv6Address EmberZclBindingEntry_t::address |
EmberZclApplicationDestination_t EmberZclBindingEntry_t::application |
EmberZclClusterSpec_t EmberZclBindingEntry_t::clusterSpec |
A cluster specification of binding.
union { ... } EmberZclBindingEntry_t::data |
struct { ... } EmberZclBindingEntry_t::destination |
EmberZclEndpointId_t EmberZclBindingEntry_t::endpointId |
An endpoint identifier of binding.
struct { ... } EmberZclBindingEntry_t::network |
uint16_t EmberZclBindingEntry_t::port |
EmberZclReportingConfigurationId_t EmberZclBindingEntry_t::reportingConfigurationId |
A reporting configuration of binding.
EmberZclScheme_t EmberZclBindingEntry_t::scheme |
EmberZclNetworkDestinationType_t EmberZclBindingEntry_t::type |
EmberZclUid_t EmberZclBindingEntry_t::uid |
The documentation for this struct was generated from the following file:
zcl-core-types.h