USB_EndpointDescriptor_TypeDef Struct Reference
USB Endpoint Descriptor.
#include <
em_usb.h
>
Data Fields | |
uint8_t | bLength |
uint8_t | bDescriptorType |
uint8_t | bEndpointAddress |
uint8_t | bmAttributes |
uint16_t | wMaxPacketSize |
uint8_t | bInterval |
Field Documentation
uint8_t USB_EndpointDescriptor_TypeDef::bDescriptorType |
Constant ENDPOINT Descriptor Type
uint8_t USB_EndpointDescriptor_TypeDef::bEndpointAddress |
The address of the endpoint
Referenced by USBD_Init().
uint8_t USB_EndpointDescriptor_TypeDef::bInterval |
Interval for polling EP for data transfers
uint8_t USB_EndpointDescriptor_TypeDef::bLength |
Size of this descriptor in bytes
uint8_t USB_EndpointDescriptor_TypeDef::bmAttributes |
This field describes the endpoint attributes
Referenced by USBD_Init().
uint16_t USB_EndpointDescriptor_TypeDef::wMaxPacketSize |
Maximum packet size for the endpoint
Referenced by USBD_Init().
The documentation for this struct was generated from the following file:
em_usb.h