EmberChildEntry Struct Reference
#include <
network-management.h
>
Data Fields | |
uint16_t | flags |
uint8_t | macExtendedId [8] |
uint32_t | timeoutSeconds |
uint16_t | secondsSinceLastTransaction |
int8_t | rssi |
Field Documentation
uint16_t EmberChildEntry::flags |
uint8_t EmberChildEntry::macExtendedId[8] |
int8_t EmberChildEntry::rssi |
uint16_t EmberChildEntry::secondsSinceLastTransaction |
uint32_t EmberChildEntry::timeoutSeconds |
The documentation for this struct was generated from the following file:
network-management.h