DTLS API
Macros |
|
| #define | EMBER_DTLS_MODE_CERT 0x01 |
|
Define the various modes of a DTLS connection.
|
|
| #define | EMBER_DTLS_MODE_PSK 0x02 |
| #define | EMBER_DTLS_MODE_PKEY 0x04 |
Typedefs |
|
| typedef uint8_t | EmberDtlsMode |
Functions |
|
| void | emberSetDtlsDeviceCertificate (const CertificateAuthority **certAuthority, const DeviceCertificate *deviceCert) |
|
Set a device certificate to be used to create a certificate based secure session on the application. The expected arguments are DER encoded X.509 certificates. If this succeeds,
emberSetDtlsDeviceCertificateReturn
should return 0.
|
|
| void | emberSetDtlsDeviceCertificateReturn (uint32_t result) |
|
Provides the result of a call to
emberSetDtlsDeviceCertificate()
.
|
|
| void | emberSetDtlsPresharedKey (const uint8_t *key, uint8_t keyLength, const uint8_t *identity, uint8_t identityLength, const EmberIpv6Address *remoteAddress) |
|
Set a key to be used to create a PSK based secure session on the application. The maximum length of the key is 32 bytes.
|
|
| void | emberSetDtlsPresharedKeyReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetDtlsPresharedKey()
.
|
|
| void | emberOpenDtlsConnection ( EmberDtlsMode dtlsMode, const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
|
Establish a DTLS connection with a peer on the Thread network. When established, this session can be used to send secure CoAP data. The device requesting the connection acts as a DTLS client.
|
|
| void | emberOpenDtlsConnectionReturn (uint32_t result, const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
|
Provides the result of a call to
emberOpenDtlsConnection()
.
|
|
| void | emberDtlsSecureSessionEstablished (uint8_t flags, uint8_t sessionId, const EmberIpv6Address *localAddress, const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
|
Indicates to the application that a secure connection was successfully established.
|
|
| uint8_t | emberGetSecureDtlsSessionId (const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
|
Request the session ID given connection parameters.
|
|
| uint8_t | emberGetDtlsConnectionNextSessionId (uint8_t sessionId) |
|
Request the next session ID following the given one. If EMBER_NULL_SESSION_ID is passed, then the first session ID is returned.
|
|
| EmberStatus | emberGetDtlsConnectionPeerPublicKeyBySessionId (const uint8_t sessionId, uint8_t *publicKey, const uint16_t publicKeyMaxSize, uint16_t *publicKeySize) |
|
Request the public key associated with a particular session.
|
|
| void | emberCloseDtlsConnection (uint8_t sessionId) |
|
Close a currently active secure session on the application. When successful, emberCloseDtlsConnectionReturn should be called on both ends of the connection with
EMBER_SUCCESS
.
|
|
| void | emberCloseDtlsConnectionReturn (uint8_t sessionId, EmberStatus status) |
|
Provides the result of a call to
emberCloseDtlsConnection()
, or indicates that the connection was closed on the other end.
|
|
| bool | emberDtlsTransmitHandler (const uint8_t *payload, uint16_t payloadLength, const EmberIpv6Address *localAddress, uint16_t localPort, const EmberIpv6Address *remoteAddress, uint16_t remotePort, void *transmitHandlerData) |
Public DTLS transmit handler to be set in emberCoapSend. The secure payload is delivered via emberProcessCoap on the other end, with a matching session ID in the transmitHandlerData of its CoapRequestInfo. See
emberProcessCoap
(
stack/include/coap.h
)
|
|
Detailed Description
See
dtls.h
for source code.
Macro Definition Documentation
| #define EMBER_DTLS_MODE_CERT 0x01 |
Note: Please configure either the CERT or PSK modes, as the public key option is currently unavailable.
| #define EMBER_DTLS_MODE_PKEY 0x04 |
| #define EMBER_DTLS_MODE_PSK 0x02 |
Typedef Documentation
| typedef uint8_t EmberDtlsMode |
Function Documentation
| void emberCloseDtlsConnection | ( | uint8_t |
sessionId
|
) |
- Parameters
-
sessionIdsessionId used for secure CoAP transport.
| void emberCloseDtlsConnectionReturn | ( | uint8_t |
sessionId,
|
| EmberStatus |
status
|
||
| ) |
- Parameters
-
sessionIdsessionId used for secure CoAP transport. status- EMBER_SUCCESS - Successfully closed the connection
- EMBER_INVALID_CALL - Invalid session ID
- EMBER_ERR_FATAL - Fatal error closing the connection
| void emberDtlsSecureSessionEstablished | ( | uint8_t |
flags,
|
| uint8_t |
sessionId,
|
||
| const EmberIpv6Address * |
localAddress,
|
||
| const EmberIpv6Address * |
remoteAddress,
|
||
| uint16_t |
localPort,
|
||
| uint16_t |
remotePort
|
||
| ) |
- Parameters
-
flags1 = server, 0 = client (possibly other info later) sessionIdsessionId used for secure CoAP transport localAddresslocal IPv6 address remoteAddressremote IPv6 address localPortlocal port remotePortremote port
| bool emberDtlsTransmitHandler | ( | const uint8_t * |
payload,
|
| uint16_t |
payloadLength,
|
||
| const EmberIpv6Address * |
localAddress,
|
||
| uint16_t |
localPort,
|
||
| const EmberIpv6Address * |
remoteAddress,
|
||
| uint16_t |
remotePort,
|
||
| void * |
transmitHandlerData
|
||
| ) |
- Parameters
-
payloadCoAP payload to be sent securely payloadLengthpayload length localAddresslocal IPv6 address localPortlocal port remoteAddressremote IPv6 address remotePortremote port transmitHandlerDatasession ID of the secure connection (see emberDtlsSecureSessionEstablished or emberGetSecureDtlsSessionId above)
| uint8_t emberGetDtlsConnectionNextSessionId | ( | uint8_t |
sessionId
|
) |
- Parameters
-
sessionIdsession ID to be followed
| EmberStatus emberGetDtlsConnectionPeerPublicKeyBySessionId | ( | const uint8_t |
sessionId,
|
| uint8_t * |
publicKey,
|
||
| const uint16_t |
publicKeyMaxSize,
|
||
| uint16_t * |
publicKeySize
|
||
| ) |
- Parameters
-
sessionIdsession ID of interest publicKeyArray that will store the public key publicKeyMaxSizeMaximum size of the array publickeySizeSize of the array in use
| uint8_t emberGetSecureDtlsSessionId | ( | const EmberIpv6Address * |
remoteAddress,
|
| uint16_t |
localPort,
|
||
| uint16_t |
remotePort
|
||
| ) |
- Parameters
-
remoteAddressremote IPv6 address localPortlocal port remotePortremote port
| void emberOpenDtlsConnection | ( | EmberDtlsMode |
dtlsMode,
|
| const EmberIpv6Address * |
remoteAddress,
|
||
| uint16_t |
localPort,
|
||
| uint16_t |
remotePort
|
||
| ) |
(For DotDot applications, the local port and remote port are both EMBER_COAP_SECURE_PORT )
- Parameters
-
dtlsModeDTLS connection mode (see EMBER_DTLS_MODE_* above) remoteAddressIPv6 address of the server localPortlocal port remotePortremote port
| void emberOpenDtlsConnectionReturn | ( | uint32_t |
result,
|
| const EmberIpv6Address * |
remoteAddress,
|
||
| uint16_t |
localPort,
|
||
| uint16_t |
remotePort
|
||
| ) |
- Parameters
-
resulterror code - an EmberStatus value if using Silicon Labs TLS
- an mbed TLS error code if using mbed TLS library (see mbedtls:include/mbedtls/ssl.h)
remoteAddressIPv6 address of the server localPortlocal port remotePortremote port
| void emberSetDtlsDeviceCertificate | ( | const CertificateAuthority ** |
certAuthority,
|
| const DeviceCertificate * |
deviceCert
|
||
| ) |
- Parameters
-
certAuthoritythe certificate authority deviceCertthe certificate
| void emberSetDtlsDeviceCertificateReturn | ( | uint32_t |
result
|
) |
- Parameters
-
result- ::0 The certificate was set successfully.
-
::result error code
- an EmberStatus value if using Silicon Labs TLS
- an mbed TLS error code if using mbed TLS library (see mbedtls:include/mbedtls/ssl.h)
| void emberSetDtlsPresharedKey | ( | const uint8_t * |
key,
|
| uint8_t |
keyLength,
|
||
| const uint8_t * |
identity,
|
||
| uint8_t |
identityLength,
|
||
| const EmberIpv6Address * |
remoteAddress
|
||
| ) |
Note: Up to 32 pre-shared keys can be stored.
If this succeeds, emberSetDtlsPresharedKeyReturn will return EMBER_SUCCESS. Otherwise, a failure status is indicated.
- Parameters
-
keythe pre-shared key keyLengthkey length keythe pre-shared identity keyLengthidentity length remoteAddressIPv6 address of peer
| void emberSetDtlsPresharedKeyReturn | ( | EmberStatus |
status
|
) |
- Parameters
-
result- ::status An EmberStatus value