power-meter API Callbacks
Functions |
|
| void | halPowerMeterOverHeatStatusChangeCallback (uint8_t status) |
|
Called upon the status change of over heat condition.
|
|
| void | halPowerMeterOverCurrentStatusChangeCallback (uint8_t status) |
|
Called upon the status change of over current condition.
|
|
| void | halPowerMeterCalibrationFinishedCallback (uint16_t gainSetting) |
|
Called when calibration is complete.
|
|
Detailed Description
These callbacks were contributed by the power-meter API.
Function Documentation
| void halPowerMeterCalibrationFinishedCallback | ( | uint16_t |
gainSetting
|
) |
This function is called upon a calibration procedure is done.
- Parameters
-
gainSettinggain setting
| void halPowerMeterOverCurrentStatusChangeCallback | ( | uint8_t |
status
|
) |
This function is called upon the status change of over current condition.
- Parameters
-
statusOVER_CURRENT_TO_NORMAL (0):changed from over current to normal; NORMAL_TO_OVER_CURRENT (1):over current occurred.
| void halPowerMeterOverHeatStatusChangeCallback | ( | uint8_t |
status
|
) |
This function is called upon the status change of over heat condition.
- Parameters
-
statusOVER_HEAT_TO_NORMAL (0):changed from over heat to normal; NORMAL_TO_OVER_HEAT (1):over heat occurred.