EmberUdpConnectionData Struct Reference
Data stored for each connection.
#include <
udp-peer.h
>
Data Fields | |
EmberUdpConnectionHandle | connection |
uint16_t | flags |
uint16_t | internal |
uint8_t | localAddress [16] |
uint8_t | remoteAddress [16] |
uint16_t | localPort |
uint16_t | remotePort |
Field Documentation
EmberUdpConnectionHandle EmberUdpConnectionData::connection |
uint16_t EmberUdpConnectionData::flags |
uint16_t EmberUdpConnectionData::internal |
uint8_t EmberUdpConnectionData::localAddress[16] |
uint16_t EmberUdpConnectionData::localPort |
uint8_t EmberUdpConnectionData::remoteAddress[16] |
uint16_t EmberUdpConnectionData::remotePort |
The documentation for this struct was generated from the following file:
udp-peer.h