Structure that holds information about a routing table entry for use on the application. See emberGetRipEntry.
#include <network-management.h
>
uint8_t EmberRipEntry::age |
uint8_t EmberRipEntry::incomingLinkQuality |
uint8_t EmberRipEntry::macExtendedId[8] |
bool EmberRipEntry::mleSync |
uint8_t EmberRipEntry::nextHopIndex |
uint8_t EmberRipEntry::outgoingLinkQuality |
uint8_t EmberRipEntry::ripMetric |
int8_t EmberRipEntry::rollingRssi |
uint8_t EmberRipEntry::routeDelta |
The documentation for this struct was generated from the following file: