EmberCoapSendInfo Struct Reference
Optional information when sending a message.
#include <
coap.h
>
Data Fields |
|
| bool | nonConfirmed : 1 |
| bool | multicastLoopback : 1 |
| EmberIpv6Address | localAddress |
| uint16_t | localPort |
| uint16_t | remotePort |
| const EmberCoapOption * | options |
| uint8_t | numberOfOptions |
| uint32_t | responseTimeoutMs |
| const uint8_t * | responseAppData |
| uint16_t | responseAppDataLength |
| EmberCoapTransmitHandler | transmitHandler |
| void * | transmitHandlerData |
| uint8_t | hopLimit |
For all fields a value of 0 or NULL means that the default will be used.
Multicast are always sent as unconfirmed.
Field Documentation
| uint8_t EmberCoapSendInfo::hopLimit |
Hop limit for multicast messages. Defaults to MPL_DEFAULT_HOP_LIMIT when set to 0
| EmberIpv6Address EmberCoapSendInfo::localAddress |
Default is to let the IP stack choose
| uint16_t EmberCoapSendInfo::localPort |
Defaults to the CoAP port (5683)
| bool EmberCoapSendInfo::multicastLoopback |
Defaults to not looping back
| bool EmberCoapSendInfo::nonConfirmed |
Defaults to confirmed
| uint8_t EmberCoapSendInfo::numberOfOptions |
Defaults to zero
| const EmberCoapOption * EmberCoapSendInfo::options |
Defaults to NULL
| uint16_t EmberCoapSendInfo::remotePort |
Defaults to the CoAP port (5683)
| const uint8_t* EmberCoapSendInfo::responseAppData |
Defaults to NULL
| uint16_t EmberCoapSendInfo::responseAppDataLength |
Defaults to zero
| uint32_t EmberCoapSendInfo::responseTimeoutMs |
Default is 'EMBER_COAP_DEFAULT_TIMEOUT_MS'
| EmberCoapTransmitHandler EmberCoapSendInfo::transmitHandler |
Defaults to using UDP
| void* EmberCoapSendInfo::transmitHandlerData |
Defaults to NULL
The documentation for this struct was generated from the following file:
-
coap.h