Commissioning
Commissioning Utilities.
Enumerations | |
enum | { EMBER_NO_COMMISSIONER = 0, EMBER_HAVE_COMMISSIONER = BIT(0), EMBER_AM_COMMISSIONER = BIT(1), EMBER_JOINING_ENABLED = BIT(2), EMBER_JOINING_WITH_EUI_STEERING = BIT(3) } |
Flag values for emberCommissionerStatusHandler(). | |
enum | EmberJoiningMode { EMBER_NO_JOINING, EMBER_JOINING_ALLOW_ALL_STEERING, EMBER_JOINING_ALLOW_EUI_STEERING, EMBER_JOINING_ALLOW_SMALL_EUI_STEERING } |
Joining modes, passed to emberSetJoiningMode() on the commissioner. No change takes place until emberSendSteeringData() is called. If steering is used, the EUI-64s of the joining devices should be passed to emberAddSteeringEui64() before calling emberSendSteeringData(). |
Functions | |
void | emberBecomeCommissioner (const uint8_t *deviceName, uint8_t deviceNameLength) |
This function petitions to make this device the commissioner for the network. This will succeed if there is no active commissioner and fail if there is one. | |
void | emberBecomeCommissionerReturn (EmberStatus status) |
Return call for emberBecomeCommissioner(). The status is EMBER_SUCCESS if a petition was sent or EMBER_ERR_FATAL if some temporary resource shortage prevented doing so. | |
void | emberStopCommissioning (void) |
This function causes this device to cease being the active commissioner. This call always succeeds and has no return. | |
void | emberGetCommissioner (void) |
This function causes the stack to call emberCommissionerStatusHandler() to report the current commissioner status. This always succeeds and has no return. | |
void | emberAllowNativeCommissioner (bool on) |
This function causes the stack to allow a connection to a native commissioner. | |
void | emberAllowNativeCommissionerReturn (EmberStatus status) |
This function provides the result of a call to emberAllowNativeCommissioner(): either EMBER_SUCCESS or EMBER_INVALID_CALL. | |
void | emberSetCommissionerKey (const uint8_t *commissionerKey, uint8_t commissionerKeyLength) |
This function sets the key that a native commissioner must use to establish a connection to a Thread router. The commissionerKey argument is known as the "commissioning credential" in the Thread spec and must be between 6 and 255 bytes in length. Internally, it is hashed to derive the 16-byte Pre-Shared Key for the commissioner, known as the PSKc. | |
void | emberSetCommissionerKeyReturn (EmberStatus status) |
This function provides the result of a call to emberSetCommissionerKey(): either EMBER_SUCCESS or EMBER_INVALID_CALL. | |
void | emberSetPskcHandler (const uint8_t *pskc) |
Handler to let application know that a PSKc TLV was successfully set. | |
void | emberCommissionerStatusHandler (uint16_t flags, const uint8_t *commissionerName, uint8_t commissionerNameLength) |
This function reports on the current commissioner state. | |
void | emberSetJoiningMode (EmberJoiningMode mode, uint8_t length) |
This function sets the joining mode, clearing the steering data if steering is to be used. | |
void | emberAddSteeringEui64 (const EmberEui64 *eui64) |
This function adds the given EUI64 to the steering data if this device is the active commissioner; has no effect otherwise. | |
void | emberSendSteeringData (void) |
This function sends the current steering data to the network, enabling joining in the process. | |
void | emberSendSteeringDataReturn (EmberStatus status) |
This function provides the result of a call to emberSendSteeringData(). | |
void | emberSetJoinKey (const EmberEui64 *eui64, const uint8_t *key, uint8_t keyLength) |
This function supplies the commissioner with the key a joining node will be using. | |
void | emberSetJoinKeyReturn (EmberStatus status) |
This function provides the result of a call to emberSetJoinKey(). | |
void | emberEnableHostDtlsClient (bool enable) |
This function allows DTLS implementations on the host. | |
void | emberCommissionNetwork (uint8_t preferredChannel, uint32_t fallbackChannelMask, const uint8_t *networkId, uint8_t networkIdLength, uint16_t panId, const uint8_t *ulaPrefix, const uint8_t *extendedPanId, const EmberKeyData *key, uint32_t keySequence) |
This function commissions the network. | |
void | emberCommissionNetworkReturn (EmberStatus status) |
This function provides the result of a call to emberCommissionNetwork. |
Detailed Description
See network-management.h
for source code.
Enumeration Type Documentation
anonymous enum |
enum EmberJoiningMode |
Function Documentation
void emberAddSteeringEui64 | ( | const EmberEui64 * | eui64 | ) |
The steering data is a Bloom filter for the EUI64s of the devices that are expected to join the network. Each added EUI64 is passed to a hash function to choose a set of bits in the filter, and those bits are set. Each potential joiner can then hash their own EUI64 and check if the resulting bits are set in the advertised filter. If so, the device is (probably) expected to join; if not, it definitely is not expected to join.
void emberAllowNativeCommissioner | ( | bool | on | ) |
Note: This call must be made on the leader before forming a network.
- Parameters
-
on
Enable / disable connections to native commissioners
void emberAllowNativeCommissionerReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberAllowNativeCommissioner(): either EMBER_SUCCESS or EMBER_INVALID_CALL.
void emberBecomeCommissioner | ( | const uint8_t * | deviceName, |
uint8_t | deviceNameLength |
||
) |
- Parameters
-
deviceName
A name for this device as a human-readable string. If this device becomes the commissioner this name is sent to any other would-be commissioners so that the user can identify the current commissioner. deviceNameLength
The length of the name.
void emberBecomeCommissionerReturn | ( | EmberStatus | status | ) |
void emberCommissionerStatusHandler | ( | uint16_t | flags, |
const uint8_t * | commissionerName, |
||
uint8_t | commissionerNameLength |
||
) |
- Parameters
-
flags
A combination of zero or more of the following: - EMBER_HAVE_COMMISSIONER a commissioner is active in the network
- EMBER_AM_COMMISSIONER this device is the active commissioner if emberStopCommissioning is called, then this flag is not returned as we are open to commissioner petitions
- EMBER_JOINING_ENABLED joining is enabled
- EMBER_JOINING_WITH_EUI_STEERING steering data restricts which devices can join. if not set, no restriction, any device can join (significant only when EMBER_JOINING_ENABLED is set)
commissionerName
The name of the active commissioner, or NULL if there is none or the name is not known. commissionerNameLength
The length of commissonerName.
This function reports on the current commissioner state.
- Parameters
-
flags
A combination of zero or more of the following: - EMBER_HAVE_COMMISSIONER a commissioner is active in the network
- EMBER_AM_COMMISSIONER this device is the active commissioner if emberStopCommissioning is called, then this flag is not returned as we are open to commissioner petitions
- EMBER_JOINING_ENABLED joining is enabled
- EMBER_JOINING_WITH_EUI_STEERING steering data restricts which devices can join. if not set, no restriction, any device can join (significant only when EMBER_JOINING_ENABLED is set)
commissionerName
The name of the active commissioner, or NULL if there is none or the name is not known. commissionerNameLength
The length of commissonerName.
void emberCommissionNetwork | ( | uint8_t | preferredChannel, |
uint32_t | fallbackChannelMask, |
||
const uint8_t * | networkId, |
||
uint8_t | networkIdLength, |
||
uint16_t | panId, |
||
const uint8_t * | ulaPrefix, |
||
const uint8_t * | extendedPanId, |
||
const EmberKeyData * | key, |
||
uint32_t | keySequence |
||
) |
This call must be made prior to calling emberJoinCommissioned(). It will not be successful if the node is already on a network.
All options except panId are REQUIRED. If a REQUIRED option is not provided, the callback emberJoinNetworkReturn will be sent to the app with an EMBER_BAD_ARGUMENT status.
Notes: If preferredChannel is 0, EMBER_ALL_802_15_4_CHANNELS_MASK is used instead of fallbackChannelMask. If preferredChannel is valid, it will automatically be added to the fallbackChannelMask.
- Parameters
-
preferredChannel
[the preferred channel] fallbackChannelMask
[the fallback channel mask] networkId
[the network ID] networkIdLength
[the string length of networkId] panId
[the short pan ID] ulaPrefix
[the 8-byte ULA prefix] extendedPanId
[the 8-byte extended pan ID] key
[the master key] keySequence
[starting key sequence, default: 0]
void emberCommissionNetworkReturn | ( | EmberStatus | status | ) |
Returns EMBER_SUCCESS if successful EMBER_BAD_ARGUMENT if any of the options are wrong EMBER_INVALID_CALL if the node is already on a network
- Parameters
-
status
Whether the call to emberCommissionNetwork was successful
This function provides the result of a call to emberCommissionNetwork.
Returns EMBER_SUCCESS if successful EMBER_BAD_ARGUMENT if any of the options are wrong EMBER_INVALID_CALL if the node is already on a network
- Parameters
-
status
Whether the call to emberCommissionNetwork was successful
void emberEnableHostDtlsClient | ( | bool | enable | ) |
This call is made in order to force the host to interface with an external commissioner if available, or use DTLS capabilities on the host (if they exist) for Thread joining or other security handshakes.
This is enabled by default for the Thread Border Router implementation. However, if the device (Border Router or otherwise) wants to use existing DTLS capabilities on the NCP stack, such as for joining, this should be toggled to false.
- Parameters
-
enable
If true, this call allows the host to perform DTLS.
void emberGetCommissioner | ( | void |
| ) |
void emberSendSteeringData | ( | void |
| ) |
void emberSendSteeringDataReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSendSteeringData().
void emberSetCommissionerKey | ( | const uint8_t * | commissionerKey, |
uint8_t | commissionerKeyLength |
||
) |
Note: This call must be made on the leader before forming a network, or on an on-mesh commissioner that wants to set the PSKc in the active dataset.
- Parameters
-
commissionerKey
the key commissionerKeyLength
key length
void emberSetCommissionerKeyReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetCommissionerKey(): either EMBER_SUCCESS or EMBER_INVALID_CALL.
void emberSetJoiningMode | ( | EmberJoiningMode | mode, |
uint8_t | length |
||
) |
No change takes place until emberSendSteeringData() is called. If steering is used, the EUI-64s of the joining devices should be passed to emberAddSteeringEui64() before calling emberSendSteeringData().
- Parameters
-
mode
The joining mode length
The length in bytes of the Bloom filter to be included in the Steering Data TLV. This field is only applicable when mode is set to EMBER_JOINING_ALLOW_EUI_STEERING. Refer to the Thread specification for details on the Bloom filter and the probability of collisions given the number of bits in the Bloom filter and the number of identifiers included.
void emberSetJoinKey | ( | const EmberEui64 * | eui64, |
const uint8_t * | key, |
||
uint8_t | keyLength |
||
) |
- Parameters
-
eui64
The EUI64 of the next node expected to join. NULL may be used if the EUI64 is not known. key
The joining key that the device will be using. keyLength
The length of the joining key.
void emberSetJoinKeyReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetJoinKey().
void emberSetPskcHandler | ( | const uint8_t * | pskc | ) |
- Parameters
-
pskc
PSKc: 16 bytes in length
void emberStopCommissioning | ( | void |
| ) |
When this call is made, emberCommissionerStatusHandler will not return the EMBER_AM_COMMISSIONER flag anymore.