Definition of the standalone bootloader interface.
Macros |
|
| #define | NO_BOOTLOADER_MODE 0xFF |
|
Define a numerical value for NO BOOTLOADER mode. In other words, the bootloader should not be run.
|
|
| #define | STANDALONE_BOOTLOADER_NORMAL_MODE 1 |
|
Define a numerical value for the normal bootloader mode.
|
|
| #define | STANDALONE_BOOTLOADER_RECOVERY_MODE 0 |
|
Define a numerical value for the recovery bootloader mode.
|
|
Functions |
|
| uint16_t | halGetStandaloneBootloaderVersion (void) |
|
Detects if the standalone bootloader is installed, and if so returns the installed version.
|
|
| EmberStatus | halLaunchStandaloneBootloader (uint8_t mode) |
|
Quits the current application and launches the standalone bootloader (if installed). The function returns an error if the standalone bootloader is not present.
|
|
Detailed Description
Definition of the standalone bootloader interface.
Some functions in this file return an
EmberStatus
value. See
error-def.h
for definitions of all
EmberStatus
return values.
See
bootloader-interface-standalone.h
for source code.
Macro Definition Documentation
◆ NO_BOOTLOADER_MODE
| #define NO_BOOTLOADER_MODE 0xFF |
Define a numerical value for NO BOOTLOADER mode. In other words, the bootloader should not be run.
◆ STANDALONE_BOOTLOADER_NORMAL_MODE
| #define STANDALONE_BOOTLOADER_NORMAL_MODE 1 |
Define a numerical value for the normal bootloader mode.
◆ STANDALONE_BOOTLOADER_RECOVERY_MODE
| #define STANDALONE_BOOTLOADER_RECOVERY_MODE 0 |
Define a numerical value for the recovery bootloader mode.
Function Documentation
◆ halGetStandaloneBootloaderVersion()
| uint16_t halGetStandaloneBootloaderVersion | ( | void |
|
) |
Detects if the standalone bootloader is installed, and if so returns the installed version.
A returned version of 0x1234 would indicate version 1.2 build 34
- Returns
- BOOTLOADER_INVALID_VERSION if the standalone bootloader is not present, or the version of the installed standalone bootloader.
◆ halLaunchStandaloneBootloader()
| EmberStatus halLaunchStandaloneBootloader | ( | uint8_t |
mode
|
) |
Quits the current application and launches the standalone bootloader (if installed). The function returns an error if the standalone bootloader is not present.
- Parameters
-
modeControls the mode in which the standalone bootloader will run. See the bootloader Application Note for full details. Options are: - STANDALONE_BOOTLOADER_NORMAL_MODE Will listen for an over-the-air image transfer on the current channel with current power settings.
- STANDALONE_BOOTLOADER_RECOVERY_MODE Will listen for an over-the-air image transfer on the default channel with default power settings.
- Returns
-
An
EmberStatuserror if the standalone bootloader is not present, or EMBER_SUCCESS .