This data structure contains a DSA signature. It is the bit concatenation of the 'r' and 's' components of the signature.

#include < ember-types.h >

Data Fields

uint8_t contents [ EMBER_SIGNATURE_SIZE ]

This data structure contains a DSA signature. It is the bit concatenation of the 'r' and 's' components of the signature.

Field Documentation

◆ contents

uint8_t EmberSignatureData::contents[ EMBER_SIGNATURE_SIZE ]

The documentation for this struct was generated from the following file:
  • ember-types.h