Defines a beacon entry that is processed when scanning, joining, or rejoining.

#include < ember-types.h >

Data Fields

uint8_t channel
uint8_t lqi
int8_t rssi
uint8_t depth
uint8_t nwkUpdateId
int8_t power
int8_t parentPriority
bool enhanced : 1
bool permitJoin : 1
bool hasCapacity : 1
EmberPanId panId
EmberNodeId sender
uint8_t extendedPanId [ EXTENDED_PAN_ID_SIZE ]

Defines a beacon entry that is processed when scanning, joining, or rejoining.

Field Documentation

◆ channel

uint8_t EmberBeaconData::channel

◆ depth

uint8_t EmberBeaconData::depth

◆ enhanced

bool EmberBeaconData::enhanced

◆ extendedPanId

uint8_t EmberBeaconData::extendedPanId[ EXTENDED_PAN_ID_SIZE ]

◆ hasCapacity

bool EmberBeaconData::hasCapacity

◆ lqi

uint8_t EmberBeaconData::lqi

◆ nwkUpdateId

uint8_t EmberBeaconData::nwkUpdateId

◆ panId

EmberPanId EmberBeaconData::panId

◆ parentPriority

int8_t EmberBeaconData::parentPriority

◆ permitJoin

bool EmberBeaconData::permitJoin

◆ power

int8_t EmberBeaconData::power

◆ rssi

int8_t EmberBeaconData::rssi

◆ sender

EmberNodeId EmberBeaconData::sender

The documentation for this struct was generated from the following file:
  • ember-types.h