#include < micro-common.h >

Data Fields

uint32_t outgoingNwkFrameCounter
uint32_t incomingParentNwkFrameCounter
uint32_t outgoingLinkKeyFrameCounter
uint32_t incomingLinkKeyFrameCounter

Field Documentation

◆ incomingLinkKeyFrameCounter

uint32_t RTCCRamData::incomingLinkKeyFrameCounter

◆ incomingParentNwkFrameCounter

uint32_t RTCCRamData::incomingParentNwkFrameCounter

◆ outgoingLinkKeyFrameCounter

uint32_t RTCCRamData::outgoingLinkKeyFrameCounter

◆ outgoingNwkFrameCounter

uint32_t RTCCRamData::outgoingNwkFrameCounter

The documentation for this struct was generated from the following file:
  • micro-common.h