The control structure for events.

#include < ember-types.h >

Data Fields

EmberEventUnits status
EmberTaskId taskid
uint32_t timeToExecute

The control structure for events.

This structure should not be accessed directly. It holds the event status (one of the EMBER_EVENT_ values) and the time left before the event fires.

Field Documentation

◆ status

EmberEventUnits EmberEventControl::status

The event's status, either inactive or the units for timeToExecute.

◆ taskid

EmberTaskId EmberEventControl::taskid

The ID of the task this event belongs to.

◆ timeToExecute

uint32_t EmberEventControl::timeToExecute

Indicates how long before the event fires. Units are milliseconds.


The documentation for this struct was generated from the following file:
  • ember-types.h