EmberEndpointDescription Struct Reference
Endpoint information (a ZigBee Simple Descriptor).
#include <
stack-info.h
>
Data Fields |
|
| uint16_t | profileId |
| uint16_t | deviceId |
| uint8_t | deviceVersion |
| uint8_t | inputClusterCount |
| uint8_t | outputClusterCount |
Endpoint information (a ZigBee Simple Descriptor).
This is a ZigBee Simple Descriptor and contains information about an endpoint. This information is shared with other nodes in the network by the ZDO.
Field Documentation
◆ deviceId
| uint16_t EmberEndpointDescription::deviceId |
The endpoint's device ID within the application profile.
◆ deviceVersion
| uint8_t EmberEndpointDescription::deviceVersion |
The endpoint's device version.
◆ inputClusterCount
| uint8_t EmberEndpointDescription::inputClusterCount |
The number of input clusters.
◆ outputClusterCount
| uint8_t EmberEndpointDescription::outputClusterCount |
The number of output clusters.
◆ profileId
| uint16_t EmberEndpointDescription::profileId |
Identifies the endpoint's application profile.
The documentation for this struct was generated from the following file:
-
stack-info.h