EmberDutyCycleLimits Struct Reference

A structure containing duty cycle limit configurations.

#include < ember-types.h >

Data Fields

EmberDutyCycleHectoPct limitThresh
EmberDutyCycleHectoPct critThresh
EmberDutyCycleHectoPct suspLimit

A structure containing duty cycle limit configurations.

All limits are absolute and are required to be as follows: suspLimit > critThresh > limitThresh For example: suspLimit = 250 (2.5%), critThresh = 180 (1.8%), limitThresh 100 (1.00%).

Field Documentation

◆ critThresh

EmberDutyCycleHectoPct EmberDutyCycleLimits::critThresh

The Critical Threshold in % * 100.

◆ limitThresh

EmberDutyCycleHectoPct EmberDutyCycleLimits::limitThresh

The Limited Threshold in % * 100.

◆ suspLimit

EmberDutyCycleHectoPct EmberDutyCycleLimits::suspLimit

The Suspended Limit (LBT) in % * 100.


The documentation for this struct was generated from the following file:
  • ember-types.h